I have a DVK-BASE-2-GEVK with MOD5031-868-2-GEVB, but the software development environment, AXGEN2 and AXRADIOLAB, don’t appear to support this combination. Is there a SDK for this combination?
I am trying to come up with a register setup for the AX5031 to achieve the following:
915 MHz carrier
Manchester encoding
ASK modulation, no shaping
1 MBPS data rate
Raw data mode, legacy mode
256 bits to transmit, which equates to 32 off 8 bit bytes
No pre or post amble.
And have come up with the following to work with the MOD5031-868-2-GEVB
PLLLOOP, 0x05
XTALOSC, 0x03
XTALCAP, 0x26
MODULATION, 0x0
MODMISC, 0x01
ENCODING, 0x08
FRAMING, 0x0
CRCINIT[0-3], 0x0
FSKDEV[0-2], 0x0
FOURFSK, 0x0
TXPWR, 0x07
TXRATELO, 0x00
TXRATEMID, 0x00
TXRATEHI, 0x10
FREQ0, 0x01
FREQ1, 0x00
FREQ2, 0x30
FREQ3, 0x39
Do the above make sense?
Regards
Bob