ON Semiconductor’s New High Efficiency Quad-Voltage Supervisor Saves Board Space and Power in Computing and Consumer Applications

PHOENIX

Share

Operating current and board space significantly reduced

Quad Voltage Supervisor ImagePHOENIX, Ariz. –– April 16, 2010 –– ON Semiconductor (Nasdaq: ONNN) a leading global supplier of high performance, energy efficient silicon solutions for green electronics, has broadened its portfolio of voltage supervisors with the introduction of the CAT8710, a much smaller and space-efficient alternative to many existing solutions. Applications for this device include computing, gaming consoles, set-top boxes, communications and industrial control equipment.

Ideal for simultaneously monitoring multiple voltages in microprocessor or ASIC based systems, the CAT8710 can be operated from a supply voltage of 1.5  to 5.5 Volts and draws just 3 micro-amperes (µA); typically consuming 10 percent of the power required for similar competing products. By integrating four voltage level monitors into a single, six-pin, SOT-23 package, the CAT8710 provides an extremely space-efficient solution that occupies approximately 25 percent of the board space compared to four individually packaged devices. ON Semiconductor has ensured maximum flexibility for design engineers by incorporating two factory preset thresholds for monitoring 3.3V, 3.0V, 2.5V and 1.8V supplies within ±5 percent, and two that are customer programmable using external resistors and adjustable down to 0.62V.

“Space and power efficiency are the two most important considerations in the latest generation product designs,” said Thruston Awalt, product marketing manager, Configurable Analog Products, ON Semiconductor. “The CAT8710 quad-voltage supervisor excels in these two areas while also giving design engineers a high degree of flexibility with both preset and programmable monitors.”

Packaging and Pricing
The CAT8710 is available in a Pb-free, RoHS-compliant six-pin SOT-23 package and is priced at $0.56 per unit in 10,000 unit quantities. Samples are available now. Projected lead-time for production quantities is currently eight to 12 weeks after receipt of order (ARO).

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.