Share

Phoenix, AZ - July 20, 2000 - ON Semiconductor (Nasdaq: ONNN), a leading provider of analog ICs, logic ICs and discrete semiconductors for wireless and communications applications, today announced it is now offering bias resistor transistors (BRTs) in two additional packages, the SC-75, one of the smallest packages in the industry and the TO-92 package. This news comes on the heels of a recent ON Semiconductor announcement regarding other discrete semiconductors newly housed in the SC-75 package.

One of ON Semiconductor's top selling products, these BRTs are pervasive in wireless, portable and other communication applications. They are general-purpose transistors combined with two resistors in one chip. This type of integration enables designers to create more compact and cost-effective end products.

The availability of these popular devices in the SC-75 package enables the migration from the SOT-23, SC-70 or SOD-123 packages to a smaller foot print, offering a sixty percent space savings over the SOT-23 and 30 percent over the SC-70. This compact profile and footprint make products in this package a natural choice for designs with real estate constraints. Furthermore, these products offer additional options in board space savings and through-hole applications.

The newly available products are the DTA114EET1 series, DTA143EE, DTC114E Series, DTC114EET1 series, DTC114TE, and DTA114E series. The BRTs available in the SC-75 package are priced are priced at a resale value of $0.055 per 3k unit quantities. The BRTs available in the TO-92 package are priced are priced at a resale value of $0.042 per 5k unit quantities. For more information regarding ON Semiconductor's BRTs in the SC-75 and TO-92 packages please select BRT's .

About ON Semiconductor

ON Semiconductor, formerly a division of Motorola, is one of the world's largest suppliers of analog, standard logic, and discrete semiconductors for data and power management. ON Semiconductor's products include integrated circuits for high-bandwidth data applications, analog ICs for power management and low-voltage power transistors. In addition to using micropackaging technology across all product families, ON Semiconductor offers the largest selection of discrete semiconductors in a variety of surface mount and standard packages. These semiconductors turn on and connect digital electronic products to our world. ON Semiconductor is the trade name of SCG Holding Corporation's affiliate, Semiconductor Components Industries, LLC.

# # #

Motorola is a registered trademark of Motorola, Inc.

Photo available through Editorial contact.

For more information:

Paul Loughran
Media Relations Manager
ON Semiconductor
602-244-4195
Linda Capcara
Group Manager
Brodeur Worldwide
602-954-0044

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.