THE VISION SHOW – BOSTON, Massachusetts - April 14, 2014 –

Share

New configurable image sensors offer cost-effective ease-of-use while combining global shutter, low-noise, high sensitivity and high speed for fast reliable machine vision and other applications















THE VISION SHOW – BOSTON, Massachusetts - April 14, 2014 – ON Semiconductor (Nasdaq: ONNN), driving energy efficient innovations, has announced the introduction of the first devices in its new PYTHON CMOS image sensor family. With resolutions of 300 K, 500 K and 1.3 Mega pixels (MPix) respectively, the PYTHON 300, 500 and 1300 are designed to address the needs of general purpose industrial image sensing applications such as machine vision, inspection and motion monitoring, as well as security and surveillance applications including intelligent transportation systems (ITS). ON Semiconductor’s new global shutter image sensors combine flexibility in configuration and resolution with high speed and high sensitivity for the industrial imaging market.

ON Semiconductor has an already extensive patent portfolio within the image sensing space, including new coverage for in-pixel CDS (ipCDS) technology enabling global shutter imaging with Correlated Double Sampling (CDS) in a compact pixel size, resulting in CCD-like optical performance with attractive combinations of optical format and resolution. This new PYTHON pixel allows the capture of fast moving scenes without distortion by combining a read noise of less than 9 e-, with 7.7 V/lux sensitivity and frame rates as high as 850 frames per second. A highly configurable sequencer also allows designers to tailor the sensor operation to the exact needs of the application, including support for fast on the fly updates to the sensor configuration. Operational support across the -40°C to +85°C industrial temperature range further underlines PYTHON’s versatility.

The new VGA, SVGA and SXGA are the first three sensors in the PYTHON family, with additional higher resolutions planned for release in the near future. All are pin-to-pin compatible with one-another and with the existing VITA1300 image sensor. The result is a hardware scalable product family where all sensors have the same data, control and optical interface, allowing camera vendors to rapidly roll-out multiple resolutions to the market with minimized development effort.

“With our new PYTHON image sensors we provide a cost-effective, high performance solution that will address the needs of the growing number of image sensing applications across a range of end markets,” said Thad Smith, Director of the Image Sensor business unit at ON Semiconductor. “PYTHON offers an image sensing solution that not only provides appealing levels of speed without compromising image quality, but is also configurable and flexible enough to provide simple integration across multiple resolutions.”

For more information about the PYTHON image sensor family, visit www.onsemi.com/python.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.