ON Semiconductor Introduces Power Supply Unit for Application Microprocessors

Share

The new NCP1526 dc-dc buck converter with integrated low noise LDO, is a single-device solution that supports multimedia functions such as mobile TVs on cellular phone

PHOENIX, Ariz. – July 25, 2006 - ON Semiconductor (Nasdaq: ONNN), a leading supplier of power management solutions, today introduced the NCP1526. This high efficiency synchronous dc-dc buck (step-down) converter features an integrated low noise LDO. Offered in a unique 0.55 mm ultra-thin DFN package, it is ideal for portable applications. The device is designed to power an application microprocessor in multimedia portable devices such as portable media players (PMP), MP3 players and either DMB or DVB-H mobile TV chipsets in cellular phones.

This new NCP1526 integrated buck converter accepts input voltage from 2.7 volts (V) to 5.2 V, and features a 3.0 megahertz (MHz) buck converter that supplies a fixed output voltage with current capability of 400 milliamp (mA). The NCP1526 delivers fast transient response, making the converter ideal to power the digital core of a portable microprocessor. The device’s integrated LDO provides a 150 mA current capability and its low noise characteristic enables it to power radio frequency (RF) sensitive analog circuitry.

Adding new functions to portable products requires the power device to have a small footprint as well as a thin profile. The high frequency oscillator in the NCP1526 converter dramatically reduces the size of external components. In fact, a very small surface mount inductor of value between 1µH to 4.7 micro Henry (µH) is recommended. The device’s integrated synchronous rectifier maximizes efficiency and minimizes solution part count. The integrated regulators are packaged in a footprint of only 3 mm x 3 mm, thus saving 50 percent of board space compared to a two-chip solution. To ensure optimal component size and safe operation, value added features like soft-start, cycle-by-cycle current limiting, and thermal shutdown protection have also been integrated.

“The NCP1526 is the first integrated converter in the market that is housed in an ultra thin 0.55 mm UDFN package, which is thinner than a flip-chip package and fits nicely into a slim portable design,” said Marie Capron, ON Semiconductor’s director of Low Voltage Power Management products. “It allows designers to differentiate their products by adding an extra application processor anytime, without waiting for the upgrade of the power management unit. In the fast-turning portable market, this design flexibility helps reduces board re-design time and enables manufacturers to get their new, slim models with extra functions to the market faster than their competitors.”

The NCP1526 offers a fixed output of 1.2 V from the converter and 2.8 V from the LDO. Other output voltage options are available upon request. The device is offered in a Pb-free, 3 mm x 3 mm x 0.55 mm ultra-thin DFN-10 package. It is priced at $0.90 per unit in 3,000 unit quantities.

For additional technical information visit www.onsemi.com or contact Crystal Lam at Crystal.Lam@onsemi.com.

About ON Semiconductor
With its global logistics network and strong portfolio of power semiconductor devices, ON Semiconductor (Nasdaq: ONNN) is a preferred supplier of power solutions to engineers, purchasing professionals, distributors and contract manufacturers in the computer, cell phone, portable devices, automotive and industrial markets. For more information, please visit ON Semiconductor’s website at https://www.onsemi.com.

# # #

ON Semiconductor and the ON Semiconductor logo are registered trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the company references its website in this news release, such information on the website is not to be incorporated herein.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.