Share

NB4N507A integrated Phase Lock Loop (PLLs) is a cost-effective, configurable precision timing solution for a wide variety of consumer and networking applications

Phoenix, Ariz. – July 28, 2005 – With more than 30 years of experience designing cutting-edge, high precision, differential timing devices, ON Semiconductor (Nasdaq: ONNN) today released the NB4N507A – the first in a series of fully-integrated phase lock loop (PLL) ICs designed to replace expensive crystal oscillators for clock generation in a wide variety of consumer and networking applications. A pioneer of Positive Emitter Coupled Logic (PECL) signaling, ON Semiconductor’s latest family of PLL ICs offers performance compatible to the most widely used crystal oscillators at a fraction of the cost.

For applications ranging from VGA graphics cards to Fibre Channel clock generation, the traditional method for generating the master clock signal has been to implement a single crystal oscillator. Historically, crystal oscillatortorically, crystal oscillators have offered better jitter performance than silicon-based devices. These canned oscillators are complex to manufacture, and so, are relatively expensive and require long lead times – sometimes up to 20 weeks. ON Semiconductor’s NB4N507A is a high-performance silicon PLL that delivers jitter performance comparable to crystal oscillators but offers far more design flexibility, a lower overall cost and greatly reduced lead times. With accuracy of 100 parts per million (ppm), the NB4N507A is a preferable alternative to crystal oscillators with similar stability.

“ON Semiconductor has developed a superior silicon replacement solution for crystal oscillators,” said Bill Schromm, ON Semiconductor vice president and general manager of High Performance Analog products. “Utilizing a fully differential bipolar design methodology, ON Semiconductor’s NB4N507A PLL offers inherent noise immunity and full industrial temperature operation not obtainable by competitive CMOS PLL clock generation devices.”

About the Device
The NB4N507A generates a clock signal ranging from 50 megahertz (MHz) to 200 MHz via an inexpensive reference crystal. With a maximum root mean square (RMS) period jitter of less than 10 picoseconds (ps), it delivers half the jitter (or noise) of competitive silicon PLL products. Because the NB4N507A is fully configurable, it provides true design flexibility. For example, a single device can be used to generate different frequencies within a system and can be reused on future designs regardless of changes in timing requirements. In addition, silicon-based ICs like the NB4N507A are inherently much simpler to manufacture which leads to lower costs and vastly lower lead times.
Package and Price
The NB4N507A is available in a 16-pin SOIC package and priced at $1.50 per unit in 1,000 unit quantities. For additional information visit https://www.onsemi.com/tech or contact Prescott Sakai at prescott.sakai@onsemi.com.

About ON Semiconductor With its global logistics network and strong portfolio of power semiconductor devices, ON Semiconductor (Nasdaq: ONNN) is a preferred supplier of power solutions to engineers, purchasing professionals, distributors and contract manufacturers in the computer, cell phone, portable devices, automotive and industrial markets. For more information, please visit ON Semiconductor’s website at https://www.onsemi.com .

# # #

ON Semiconductor and the ON Semiconductor logo are registered trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the company references its website in this news release, such information on the website is not to be incorporated herein.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.