ON Semiconductor Introduces Overvoltage Protection IC with Industry’s Highest Voltage Rating and Fastest Turn-off Speed for Portable Charging Applications

Share

NCP346 withstands voltage transients up to 30 volts and steady-state voltages of 25 volts in applications with an external ac-dc adapter, a car charger accessory and/or a battery charger

PHOENIX, Ariz. – Dec. 9, 2003 - Continuing its campaign to introduce power management devices that enable designers to deliver differentiated portable products, ON Semiconductor (Nasdaq: ONNN) today introduced the NCP346 – an overvoltage protection circuit (OVP) optimized for applications with an external ac-dc adapter, a car charger accessory and/or a battery recharger. Delivering superior voltage capability and faster turn-off speed than standard CMOS supervisory circuits, the device is ideal for cell phone, digital camera, portable computer, PDA and portable CD player applications.

The NCP346 OVP circuit is a key component in a battery charging system specifically intended to protect sensitive charging electronics from high-voltage events detected on the input by quickly disconnecting them from the adapter. The rugged BiCMOS process on which the NCP346 is built enables it to turn off a series PFET in less than 1 microsecond (usec) and withstands up to 30 volts (V) of overvoltage transients (or 25 V steady state). The only competitive device options for the NCP346 are low voltage CMOS supervisors that have voltage ratings only as high as 12 V and turn-off times in the range of 200 usecs for comparable capacitive loads. ..More

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.