Share

The new series of protection diode arrays are the first in the industry to be offered in a tiny, ultra-thin SOT-953 package

PHOENIX, Ariz. – Dec. 13, 2006 - ON Semiconductor (Nasdaq: ONNN), a leading global supplier of efficient power management solutions, today introduced a new series of low-capacitance electrostatic discharge (ESD) protection arrays in an ultra-small SOT-953 package. Measuring 1.0 mm x 1.0 mm with a 0.5 mm profile, these devices are ideal for applications where board space is at a premium. Designed for a wide range of sensitive equipment, these devices are optimized for use in cell phones, PDAs, digital cameras and other protection applications.

These new SOT-953 packaged devices are 60 percent smaller than the SOT-553 ESD protection diode arrays also available from ON Semiconductor. The SOT-953 provides a 30 percent space savings compared to the 1.0 mm x 1.45 mm Micro-QFN - currently the next smallest package available in the market today.

The Devices
The NUP45V6 series offer four independent lines of protection from ESD and other harmful transient voltage events. This new series includes devices with protection voltages of 5.6 volts (V), 6.8 V and 12 V and provide IEC61000 Level 4-2 ESD performance. Because of their miniature size, these diodes can be placed near input/output ports to suppress the transient voltage before it can be coupled into the rest of the board. Delivering low capacitance of less than 7 picofarads (pF) at 3 V, and low leakage current of less than 0.1 micro Amp (µA), these integrated devices are highly efficient and offer reliable protection. The NUP45V6, NUP46V8 and NUP412V are budgetary priced of $0.12 USD in quantities of 10,000.

“By offering innovative board-level solutions like the new ultra-small packaged NUP45V6 series, ON Semiconductor directly addresses the needs of design engineers,” said Hyung-Sup Kim, ON Semiconductor’s marketing director for the Consumer Products Division. “The smaller board space consumption and low profile of the SOT-953 packaging technology, makes the new ESD arrays particularly well suited for next generation slim phones. We plan to continue to expand and adapt our handheld consumer product portfolio with targeted new devices and repackaged existing components. In this way, we can offer a broad range of efficient component solutions housed in highly desirable compact footprints.”

For additional technical information visit www.onsemi.com, or contact Kelli McNatt at Kelli.McNatt@onsemi.com.

About ON Semiconductor
With its global logistics network and strong portfolio of power semiconductor devices, ON Semiconductor (Nasdaq: ONNN) is a preferred supplier of power solutions to engineers, purchasing professionals, distributors and contract manufacturers in the computer, cell phone, portable devices, automotive and industrial markets. For more information, please visit ON Semiconductor’s website at https://www.onsemi.com.

# # #

ON Semiconductor and the ON Semiconductor logo are registered trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the company references its website in this news release, such information on the website is not to be incorporated herein.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.