ON Semiconductor Introduces Industry’s Lowest Profile ESD Protection Arrays for High Speed Data Line Protection in Portable Applications

New ESD protection devices provide 20 percent lower profile and boast 0.5 pF typical capacitance and low clamping voltage

PHOENIX, Ariz. – Sept. 24, 2008 - ON Semiconductor (Nasdaq: ONNN), a global leader in high performance, energy efficient, silicon solutions, today announced two new members of its low capacitance Electrostatic Discharge (ESD) protection product line - the NUP4016 and the ESD11L5.0D. These new products utilize ON Semiconductor’s patented, leading-edge, integrated ESD protection platform, which enhances clamping performance while maintaining ultra-low capacitance and small die size. Offered in ultra-small packages that provide a 20 percent lower profile than previous package versions, they are ideal protection devices for portable applications such as mobile phones, MP3 players, flat panel displays and other high-speed communication applications requiring superior protection in an ultra-slim package.

“The fact that portable electronics continue to shrink yet still offer added functionality isn’t news,” said Manor Narayanan, ON Semiconductor vice president and general manager of Digital Consumer Products Division. “The news is in how semiconductor solutions like ON Semiconductor’s new protection devices are helping designers find ways to incorporate world class ESD protection along with ultra low capacitance to maintain high speed data rates, without gobbling up too much valuable board area.”

The NUP4016protects four high speed data lines in the tiny 1.0 mm x 1.0 mm x 0.4 mm SOT-953 package - making it the lowest profile ESD device for high speed communication interfaces on the market today. This device also has ultra low capacitance of 0.5 pico farad (pF) per I/O line which make it suitable for protecting high speed interfaces such as USB 2.0 high speed (480 Mb/s) and HDMI (1.65 Gb/s). This small size coupled with the leading-edge capacitance and clamping voltage performance makes this device the premier solution for applications in space constrained products such as cell phones, portable MP3 players, PDAs and digital cameras.

The ESD11L5.0Dprotects two high speed data lines at 0.5 pF in the ultra small 1.0 mm x 0.6 mm x 0.37 mm SOT-1123 making it the lowest profile ESD device for high speed communication and USB 2.0 data and power line and protection available on the market today. The SOT-1123 package offers a 50 percent smaller footprint and 20 percent lower height than comparable solutions offered in a SOT-723 .Integrating ON Semiconductor’s ultra-low capacitance technology into a 3-pin package provides the designer with a solution to protect the D+ and D- lines of a USB2.0 port with a single device. The ESD11L5.0D can also be connected cathode to cathode to protect a single bi-directional line at 0.25 pF, ideal for protecting high frequency RF antenna lines.

Both the NUP4016 and ESD11L5.0D are capable of clamping an input ESD waveform of 15 kilovolt (kV) to less than 8 volts (V) in a matter of nanoseconds, ensuring the highest levels of protection for today’s ESD sensitive integrated circuits (IC). Other low capacitance off-chip ESD protection technologies, such as polymer and ceramic-based varistors, offer low capacitance, but their ESD clamping voltage is significantly higher than the ON Semiconductor solution. In addition, the ON Semiconductor silicon devices are free from wearout mechanisms that affect the reliability and performance of passive technologies after multiple surge events such as ESD.

“ON Semiconductor continues to lead the industry in delivering high performance ESD protection solutions in smaller, lower profile products that not only meet the size requirements of next generation applications, but that deliver the performance demanded by customers.,” said Gary Straker, ON Semiconductor general manager and director of Protection and Control Division. “These new devices meet the challenge of protecting sensitive components in high-speed applications from the severe damage caused by ESD.”

The NUP4016 is available in a SOT-953 package and is priced at $0.40 USD per unit in 3,000 units quantities. The ESD11L5.0D is available in a SOT-1123 package and is priced at $0.21 USD per unit in 8,000 units quantities.

For additional technical information, visit the ON Semiconductor Circuit Protection website https://www.onsemi.com/circuitprotection or contact Eric Dominguez at eric.dominguez@onsemi.com or Lon Robinson at lon.robinson@onsemi.com.

About ON Semiconductor
With its global logistics network and strong product portfolio, ON Semiconductor (Nasdaq: ONNN) is a preferred supplier of high performance, energy efficient, silicon solutions to customers in the power supply, automotive, communication, computer, consumer, medical, industrial, mobile phone, and military/aerospace markets. The company’s broad portfolio includes power, analog, DSP, mixed-signal, advance logic, clock management and standard component devices. Global corporate headquarters are located in Phoenix, Arizona. The company operates a network of manufacturing facilities, sales offices and design centers in key markets throughout North America, Europe, and the Asia Pacific regions. For more information, visit https://www.onsemi.com.

# # #

ON Semiconductor and the ON Semiconductor logo are registered trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the company references its Web site in this news release, such information on the Web site is not to be incorporated herein.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.