ON Semiconductor Introduces Industry’s Lowest Capacitance ESD Protection for High Bandwidth Interfaces

May 11, 2011

New ESD7004 delivers robust ESD protection and ultra low 0.4 pF capacitance required for high speed data interfaces such as USB 3.0 and eSATA used in notebooks and tablets

New ESD Protection Diode image

PHOENIX, Ariz. – May 11, 2011 – ON Semiconductor (Nasdaq: ONNN) a premier supplier of high performance silicon solutions for energy efficient electronics, has released its newest product for integrated electrostatic discharge (ESD) protection for use in notebooks, tablets, and external storage devices.

The new ESD7004 is specifically designed to preserve signal integrity in high speed applications such as USB 3.0 (5 gigabits per second, Gb/s) and eSATA (up to 6 Gb/s).  The device breaks the current industry capacitance barrier offering an ultra low 0.4 picofarad (pF) rating, while maintaining extremely low ESD clamping voltage.

As high speed interfaces exceed 5 Gb/s, a few tenths of a picofarad capacitance can have a major effect on the signal integrity of the data being transmitted. By lowering the capacitance down to 0.4 pF typical, 0.5 pF maximum, the ESD7004 offers an ESD protection solution that has virtually no effect on eye diagrams of USB 3.0 at 5 Gb/s and eSATA at 6 Gb/s. In addition, these parts maintain less than 1 decibel (db) insertion loss at over 8 gigahertz (GHz) during S21 measurements, ensuring negligible effect on high speed data transmission. 

“Consumer and computing products including external storage devices are adopting higher bandwidth interfaces to support increased data transfer requirements,” said Gary Straker, vice president and general manager of ON Semiconductor’s Protection Products Division. “The ESD7004 from ON Semiconductor addresses the needs of this trend by offering an ESD protection solution that protects sensitive chipsets without degrading the signal integrity of the high speed interfaces it is protecting.”  

Utilizing ON Semiconductor’s patented ESD protection silicon which incorporates innovative isolation techniques, the ESD7004 offers extremely low clamping voltages and fast response time during ESD events. These designs boast clamping voltages at 11.4 volts (V) or less during Transmission Line Pulse (TLP) +/-8 amperes (A) testing which safeguards chipsets using small geometries and low voltage tolerances, common for high speed datalines. An ESD rating of 15 kV contact per the IEC61000-4-2 standard and low turn on resistance during ESD events ensures that the most sensitive chipsets will be safe from ESD threats. 

Packaging and Pricing
This ESD7004 is offered in the popular uDFN 2.5 mm x 1.0 mm x 0.5 mm 10-pin package which integrates 4 lines of protection in a flow through routing pinout that enable board designers to route traces easily with minimal impact to impedance matching. Budgetary pricing for this device is $0.097 per unit in 10,000 unit quantities.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.