ON Semiconductor Introduces Industry’s Fastest High Gain Oscillator Amplifier/Buffer for Networking and Telecom Applications

Share

The NBLVEP16VR amplifier enables high gain outputs and a fully differential feedback loop at a maximum speed of 2.5 GHz for timing modules

Phoenix, Ariz. – Jan. 12, 2004 – Continuing to expand its portfolio of advanced components for high-speed data and telecommunication applications, ON Semiconductor (NASDAQ: ONNN) today introduced the NBLVEP16VR - an amplifier featuring both an oscillator gain stage and enabled high gain outputs.

Delivering operating frequencies above 2.5 gigahertz (GHz), the device is ideal for timing module applications in high-speed telecommunications, networking and automated test equipment. Specific applications include use in the buffer/amplifier for Voltage Controlled Crystal Oscillators (VCXO), Temperature Compensated Crystal Oscillators (TCXO) and Surface Acoustic Wave (SAW) based modules in high-speed telecommunications, networking and automated test equipment... More

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.