ON Semiconductor Introduces Automotive Grade Non-Synchronous Boost Controller with Wide Input Range

PHOENIX, Ariz. – August 22, 2011 –

Share

Feature-rich device incorporates multiple protection functions and offers flexibility for automotive designs

NCV8871 non-synchronous boost controller

PHOENIX, Ariz. – August 22, 2011 – ON Semiconductor (Nasdaq: ONNN), a premier supplier of high performance silicon solutions for energy efficient electronics, today introduced a new adjustable output non-synchronous boost controller for automotive systems.

The NCV8871 is a wide input voltage device, with a range of 3.2 volts (V) to 44 V, which can be used to drive an external N−channel MOSFET. The device incorporates an internal regulator that supplies charge to the gate driver. This new boost controller has a 3.0 microampere (µA) quiescent current when in sleep mode, allowing power consumption to be minimized. It features a synchronizable switching frequency, with two available versions that can be set at 170 kHz typical, or 1 MHz typical. Peak current mode control with internal slope compensation ensures device stability over the wide automotive battery range. This also ensures the device is protected during a current fault condition by turning off the power switch for the remainder of the cycle if the current limit is exceeded. Further protection is provided by a thermal shutdown mechanism (with a 170 ⁰C threshold) and a 3.1 V undervoltage lockout.

The NCV8871 is highly programmable, with various other frequency options available upon request. Additional options include different slope compensation values, current limit set points, and different gate drive voltages for interfacing with various MOSFETs. The device also supports multiple topology configurations, including boost, flyback, SEPIC, and multi-phase. Output power ranges from a few watts (W) up to 200 W in a boost topology.

“The NCV8871 operates down to 3.2 V, whereas alternative controller solutions on the market typically only go down to 4 V,” said Jim Alvernaz, director of the automotive product division at ON Semiconductor. “This makes the device highly optimized for engine start/stop applications. Its high level of integration brings other benefits, too. Previously, the only option for engineers was to utilize more complex devices, which had higher pin counts and called for a larger number of external components. The NCV8871 simplifies the design process, reduces the bill of materials, and shortens the design time.”

The NCV8871 has an operating junction temperature of −40 ⁰C to 150 ⁰C. The device is offered in a Pb-free, RoHS compliant SOIC-8 package, and is priced at $0.83 per unit in quantities of 2,500 units.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.