Share

New families of bipolar LDOs deliver very high accuracy over full operating conditions and superior dynamic response for networking, computing, set-top box, gaming and display applications

PHOENIX, Ariz. – Feb. 13, 2007 - ON Semiconductor (Nasdaq: ONNN), a global leader in power management semiconductor solutions, has introduced four new high performance bipolar Low Dropout (LDO) Linear Regulators. With output currents ranging from 0.5 Amperes (A) up to 3.0 A and industry-leading low noise performance, the new NCP3335A, NCP5661, NCP565, NCP5662, and NCP5663 are ideal for use in networking, computing, set-top box, gaming, and display applications

These 1 A to 3 A linear regulators offer output voltages down to 0.9 V and employ a special composite architecture that provides extremely fast (< 1.0 micro-seconds) dynamic (a.k.a., transient) response to changing output loads. Delivering industry-leading low noise performance without the need for a bypass noise reduction capacitor, the devices help reduce overall system costs and free up valuable board space. Providing low ground current independent of output load, these devices reduce power losses. In particular, the 500 mA NCP3335A LDO can sustain inputs voltages up to 16 V and employs a special voltage reference and feedback mechanism that offers extremely tight output accuracies over operating conditions of load, line and temperature. Output accuracies for all the devices are from sub 1 percent at room temperature and sub 1.5 percent across the operating range of line, load, and temperature conditions.

The Devices
The NCP3335A is a 500 mA LDO with enable. It is available with 2.5 V, 2.85 V, 3.3 V, 5.0 V and adjustable output voltages. Offered in a Pb-free Micro8™ package, it is priced at $0.34 per unit in 4,000-unit quantities. This device is also offered in a Pb-free 3 mm x 3 mm DFN-10 package priced at $0.36 per unit in 3,000-unit quantities. Additional voltage options in both packages are in development for release in 2007.

The NCP5661 is a 1 A linear regulator with enable. It is available with 1.2 V, 1.5 V, 1.8 V, 2.5 V, 2.8 V, 3.0 V, 3.3 V and adjustable output voltages. Offered in a Pb-free DPAK package, it is priced at $0.35 per unit in 2,500-unit quantities. Also available in a Pb-free 3 mm x 3 mm DFN-6 package, it is priced at $0.53 per unit in 3,000-unit quantities.

The NCP565 is a 1.5 A linear regulator. It is available with 1.2 V, 3.3 V and adjustable output voltages. Offered in a Pb-free D2PAK package, it is priced at $0.48 per unit in 800-unit quantities. Also offered in a Pb-free 3 mm x 3 mm DFN-6 package, it is priced at $0.53 per unit in 2,000-unit quantities.

The NCP5662 is a 2 A linear regulator with enable. It is available with 1.5 V, 3.3 V and adjustable output voltages. Offered in a Pb-free D2PAK package, it is priced at $0.57 per unit in 800-unit quantities. This device family will also be available in a 4 mm x 4 mm DFN package later this year.

The NCP5663 is a 3 A linear regulator with enable. It available with 1.5 V and adjustable output voltages. Offered in a Pb-free D2PAK package, it is priced at $0.61 per unit in 800-unit quantities.

For additional technical information, visit https://www.onsemi.com. For information about additional voltage options or packages, contact Sharadh Navale at sharadh.navale@onsemi.com.

About ON Semiconductor
With its global logistics network and strong portfolio of power semiconductor devices, ON Semiconductor (Nasdaq: ONNN) is a preferred supplier of power solutions to engineers, purchasing professionals, distributors and contract manufacturers in the computer, cell phone, portable and consumer devices, automotive and industrial markets. For more information, please visit ON Semiconductor’s website at https://www.onsemi.com.

# # #

ON Semiconductor and the ON Semiconductor logo are registered trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the company references its Web site in this news release, such information on the Web site is not to be incorporated herein.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.