ON Semiconductor&#153 Expands Low Dropout Regulator Portfolio

Share

Phoenix, AZ - May 30, 2000 - ON Semiconductor (Nasdaq: ONNN), a leading provider of analog IC solutions for wireless, communications, automotive and networking and computing applications, has added the MC33275 and MC33375 low dropout voltage regulators to its already expansive power management portfolio. These new LDOs offers designers voltage and current capabilities necessary for applications that require low loss voltage conversion. They are ideal for battery powered computer, consumer and industrial equipment where an extension of battery life is desirable.

The MC33275 and MC33375 LDO regulators are medium current LDO regulators that provide fixed outputs of 2.5, 3.0, 3.3 and 5.0 volts from a maximum input of up to 13 volts and do not require large output capacitors to achieve stability of the output voltage. The devices feature a very low typical quiescent current of 125 5A and are capable of supplying output currents of up to 300mA. This very low input-to-output voltage differential coupled with the low quiescent current enable designers to use these devices in designs where the battery usage needs to be maximized. Also contained internally onboard the MC33275 and MC33275 is circuitry to provide over-current and overheating protection. Additionally, the MC33375 is equipped with an enable feature that permits added energy savings in the end product by allowing the designer the option to turn off portions of the circuitry when idle.

Both the MC33275 and MC33375 LDO regulators are packaged in compact SOT-223 and SOP-8 packages, with the MC33275 device also offered in a DPAK. These space saving packages combined with the medium current output, low dropout voltages and enable feature in the MC33375, make these devices an attractive option for system designers. They also satisfy the requirements of the growing market trend for devices with higher output currents and increasing efficiencies in smaller packages.

"The low input-to-output voltage differential and bias current specifications enable both the MC33275 and MC33375 LDO regulators to be easily designed into a wide variety of applications including battery powered portable applications where designers are looking for cost-effective ways to extend battery life in their designs," said Ralph Quinsey, general manager of ON Semiconductor's Analog Integrated Circuit Division. " Very low dropout voltage of 260mV at 300mA, low quiescent current of 125 5A, internal protection circuitry, the enable feature on the MC33375 and the miniature surface mount packages are all compelling reasons for designers to select these devices for their designs."

Samples and production quantities for the MC33275 and MC33375 LDO regulators are currently available. Suggested pricing for these devices ranges from $0.60 for 10K units. Additional technical information on this LDO series can be located at mc33275-375

About ON Semiconductor

ON Semiconductor, formerly a division of Motorola, is one of the world's largest suppliers of analog, standard logic, and discrete semiconductors for data and power management. ON Semiconductor's products include integrated circuits for high-bandwidth data applications, analog ICs for power management and low-voltage power transistors. In addition to using micropackaging technology across all product families, ON Semiconductor offers the largest selection of discrete semiconductors in a variety of surface mount and standard packages. These semiconductors turn on and connect digital electronic products to our world. ON Semiconductor is the trade name of SCG Holding Corporation's affiliate, Semiconductor Components Industries, LLC.
Further information is available at the Company's website: https://www.onsemi.com

# # #

Motorola is a registered trademark of Motorola, Inc.

Photo available through Editorial contact.

For more information:

Yinka Massally
Media Relations Manager
ON Semiconductor
602-244-6398
Linda Capcara
Group Manager
Brodeur Worldwide
602-282-5427

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.