ON Semiconductor Expands High Speed Logic Family Portfolio

Share

ON Semiconductor today introduced the second phase of the new generation of ECL based logic ICs. Known as the ECLinPS Plus series, these logic chips satisfy power supply requirements of 2.5V, 3.3V and 5V. They also offer a 30% AC performance advantage and tighter skews than comparable ECL logic series currently on the market. With system speeds now exceeding several hundred megahertz, designers have more options to choose from in creating high speed systems that require faster throughput and higher accuracy rates.

The first phase of this new ECL family - called the "Plus" series - was introduced earlier this year. ECLinPS Plus is the solution to the market demand for higher data transfer speed operation in excess of 500 MHz. This latest addition to the ECLinPS Plus family boasts enhanced functionality in addition to the faster propagation delays, rise / fall times and tighter skews than the previous ECL families.

ECLinPS Plus provides superior isolation over multiple gate logic. It is a family of single / multi (essential logic primitive) gates, multiplexers, flops, etc. that already satisfies 3.3V and 5V system requirements. Two new functions, EP111 and EP210, both timing circuits, are compatible with both 2.5V and 3.3V supplies. ON Semiconductor plans to add additional products to the portfolio. Packaged gates switch in 170ps typically with flip-flop toggle frequencies at over 3GHz utilizing the advantage of flow-through pinouts. Some of the devices are direct pin replacements to the already available ECLinPS Lite logic series. "The migration plan for ECLinPS Plus is to eventually offer products that satisfy all power supply requirements," comments Sandra Lowe, vice president and general manager of the logic products business for ON Semiconductor. "ON Semiconductor offers the only ECL product portfolio that addresses system speeds at 2.5 Gigabits and above."

As with the original ECLinPS Plus series, this latest product offering will continue to provide the adhesion for high speed systems for the future. The series will also find use in applications such as ATE systems, computer and network systems, optical data networks and high bandwidth amplifiers.

These ECLinPS Plus devices are housed in small, space saving, standard SOIC, TSSOP and TQFP packages. The small package sizes make them ideal for pin cards and other applications that require density, yet maintaining signal integrity.

This second phase of the ECLinPS Plus Logic family includes 19 new functions consisting of 10 essential logic primitives, 7 CMOS/TTL translating functions and 2 timing circuits in 8-lead SOIC/TSSOP, 20-lead TSSOP, and 32-lead TQFP packages. Most functions are in full production release today with the remaining devices being available by the end of 1999. Additional functions will be added to the ECLinPS Plus family throughout 2000. The listing of available products can be found on the ONSEMI website. Pricing is dependent on package type, device function and order quantity.

About ON Semiconductor

ON Semiconductor, formerly a division of Motorola, is the world's leading supplier of analog, logic and discrete semiconductor components with shipments of 15 billion units in 1998 totaling $1.5 billion in sales. These power and interface products are an integral part of electronics that provide the security, convenience and entertainment in today's world. ON Semiconductor is the tradename of SCG Holding Corporation. Web site: https://onsemi.com

# # #

ECLinPS Plus and ECLinPS Lite are trademarks of Semiconductor Components Industries, LLC.

Motorola is a registered trademark of Motorola, Inc.

Photo available through Editorial contact.

For more information:

Yinka Massally
Public Relations Manager
ON Semiconductor
602-244-6398
Linda Capcara
Account Director
Brodeur Worldwide
602-954-0044
Pete Weaver
Logic Marketing Manager
ON Semiconductor
602-244-3227

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.