Share

Capable of data-rates above 12 Gigabits per second, the enhanced GigaComm™ devices are ideal for high performance applications in OC-192 networking and telecommunications

PHOENIX, Ariz. – March 3, 2005 – Applying decades of expertise in high-speed clock and data management to the networking and telecommunictions markets, ON Semiconductor (Nasdaq: ONNN) today introduced the NB7L11M, NB7L14M, NB7L86M, NBSG16M, and NB7N017M – Silicon Germanium (SiGe) based, high bandwidth, fully differential clock distribution, clock driving, clock multiplexing, and clock pre-scaling ICs that support Current Mode Logic (CML) output. The devices are the newest members of the company’s GigaComm™ family of high-performance clock and data management ICs designed for the telecommunications, networking, high-end computing and automated test equipment industries.

Features and Benefits
“As designers migrate from simple CMOS solutions to the performance range dominated by bipolar ICs, Current-Mode Logic is one of the most convenient protocols for high speed interfacing and is quickly becoming the protocol of choice for emerging, high bandwidth, networking applications,” said Mike Radhanauth, ON Semiconductor director of marketing and business development for High Frequency Products.

The new GigaComm™ devices simplify initial conditions and connection termination with on-chip 50 ohm input and output termination. This allows for a point-to-point implementation expected of CMOS solutions, but uncommon in bipolar designs. Like Reduced Swing ECL (RSECL), the small 400 millivolt (mV) signal swing of CML results in reduced power consumption and rise/fall times. The irregularities that result from back reflection of signals later in the circuit - which is common to high frequency signaling - are minimized by the on-chip termination.

Capable of data-rates above 12 Gigabits per second (Gbps) in some cases, these devices are ideal for high performance applications in OC-192 applications. High speed backplane interfacing is a breeze with propagation delay below 150 picoseconds (ps) and rise and fall times below 53 ps. Combined with the design flexibility inherent in CML, the performance capability of the NBSG16M results in an optimum solution for data transmission in networking applications.

New GigaComm™ Devices
- The NB7L11M is a 12 Gbps, 8 GHz, 2.5 V or 3.3 V SiGe Differential Clock Driver that reproduces the input clock signal in the form of two identical CML output signals. In 16-pin QFN, it is priced at $25.20 per unit in 1,000 unit quantities.
- The NB7L14M is a 12 Gbps, 8 GHz, 2.5V or 3.3V SiGe Differential Clock Driver with a 1:4 fan-out and CML Outputs. In a 16-pin QFN, it is priced at $30.24 per unit in 1,000 unit quantities.
- The NBSG16M is a 10Gbps, 10GHz, 2.5 V or 3.3 V SiGe Differential Receiver/Driver with CML Outputs. In a 16-pin QFN, it is priced at $20.59 per unit in 1,000 unit quantities.
- The NB7L86M is a 12 Gbps, 8 GHz, 2.5 V or 3.3 V SiGe Differential Smart Gate with CML Outputs. It offers programmable flexibility to choose between AND/NAND, OR/NOR, XOR/XNOR or 2:1 multiplexing capabilities. It offers all of the primary logic functions at break-neck speeds for high performance applications. In a 16-pin QFN, it is priced at $13.95 per unit in 1,000 unit quantities.
- The NB7N017M is a 3.3V dual 8-bit modulus, divider/prescaler with CML outputs, capable of switching at speed greater than 3.5GHz. In a 52-pin QFN, it is priced at $23.26 per unit in 1,000 unit quantities.

Like all members of the GigaComm™ family, these devices feature ON Semiconductor’s AnyLevel™ technology which includes 50 ohms (Ω) input termination resistors and accepts all major signaling standards – specifically Negative ECL (LVNECL), PECL, LVCMOS/LVTTL, CML or LVDS.

Evaluation and demonstration boards are available for all GigaComm devices. All the devices are also available in wafer form to offer additional design flexibility.

For additional technical information or to request samples, visit https://www.onsemi.com/tech or contact Josh Warner at josh.warner@onsemi.com

About ON Semiconductor
With its global logistics network and strong portfolio of power semiconductor devices, ON Semiconductor (Nasdaq: ONNN) is a preferred supplier of power solutions to engineers, purchasing professionals, distributors and contract manufacturers in the computer, cell phone, portable devices, automotive and industrial markets. For more information, please visit ON Semiconductor’s website at https://www.onsemi.com.

# # #

ON Semiconductor and the ON Semiconductor logo are registered trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the company references its website in this news release, such information on the website is not to be incorporated herein.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.