ON Semiconductor Expands ESD Protection Portfolio with Award Winning Ultra-Low Capacitance Technology

Company maintains leadership position in high performance ESD protection solutions with industry’s lowest clamping voltage products in space saving micro packages

PHOENIX, Ariz. – June 19, 2008 - ON Semiconductor (Nasdaq: ONNN), a global leader in power management and circuit protection semiconductor solutions, today announced the expansion of its high performance off-chip ESD protection portfolio with the introduction of two best-in-class devices - the ESD7L5.0D and the NUP4212. These new products have been designed using ON Semiconductor’s propriety integrated ESD protection platform, which enhances clamping performance while maintaining low capacitance and small die size.

The ESD7L5.0D protects two high speed data lines at 0.5 pico farad (pF) capacitance per line in the tiny 1.2 mm x 1.2 mm x 0.5 mm SOT-723 package. Integrating ON Semiconductor’s low capacitance technology into a 3-pin package provides the designer with a solution to protect the D+ and D- lines of a USB2.0 port with a single device. The ESD7L5.0D can also be connected cathode to cathode to protect a single bi-directional line at 0.25 pF, ideal for protecting high frequency RF antenna lines.

The NUP4212 protects four high speed data lines at 0.7 pF per line and 2 Vcc power lines in the compact 1.6 mm x 1.6 mm x 0.5 mm UDFN-6 package. This enables the designer to protect the D+ and D- lines plus the Vcc line on two USB ports with a single integrated solution.

Both new devices share key features which distinguish the company’s proprietary technology from competitive offerings. The ESD7L5.0D and NUP4212 are capable of clamping an input ESD waveform of 15 kilovolt (kV) to less than 7 volts (V) in a matter of nanoseconds, ensuring the highest levels of protection for today’s ESD sensitive integrated circuits (IC). Other low capacitance off-chip ESD protection technologies, such as polymer and ceramic-based varistors, offer low capacitance, but their ESD clamping voltage is significantly higher than the ON Semiconductor solution. In addition, the ON Semiconductor silicon devices are free from wearout mechanisms that affect the reliability and performance of passive technologies after multiple surge events such as ESD.

“ON Semiconductor is continuing to expand its leadership in high performance ESD protection solutions with the introduction of ultra low capacitance products targeting high speed data applications,” said Mamoon Rashid, ON Semiconductor vice president and general manager of the company’s Discrete Products Division. “Next generation portable applications require improved performance and increased design flexibility at higher and higher data rates. ON Semiconductor continues to respond to this trend by introducing a complete family of low capacitance ESD protection solutions”.

The first product introduced on this technology platform, the ESD9L5.0S, was awarded Electronic Products magazine’s 2007 “Product of the Year” award for a significant advance in technology, its application and innovation in design.

The ESD7L5.0DT5G is available in a SOT-723 package and is priced at $0.20 USD per unit in 8,000 units quantities. The NUP4212 is available in a UDFN-6 package and is priced at $0.608 USD per unit in 3,000 unit quantities.

For additional technical information, visit the ON Semiconductor Circuit Protection website https://www.onsemi.com/circuitprotection or contact Lon Robinson at lon.robinson@onsemi.com or Eric Dominguez at eric.dominguez@onsemi.com.

About ON Semiconductor
With its global logistics network and strong product portfolio, ON Semiconductor (Nasdaq: ONNN) is a preferred supplier of efficient power solutions to customers in the power supply, automotive, communication, computer, consumer, medical, industrial, mobile phone, and military/aerospace markets. The company’s broad portfolio includes power, analog, DSP, mixed-signal, advance logic, clock management and standard component devices. Global corporate headquarters are located in Phoenix, Arizona. The company operates a network of manufacturing facilities, sales offices and design centers in key markets throughout North America, Europe, and the Asia Pacific regions. For more information, visit https://www.onsemi.com.

# # #

ON Semiconductor and the ON Semiconductor logo are registered trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the company references its Web site in this news release, such information on the Web site is not to be incorporated herein.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.