ON Semiconductor Expands ECLinPS MAX Clock Management Portfolio with New High Performance LVDS Fanout Buffers

Share

Increased performance levels of the clock management portfolio offer design flexibility for high performance telecommunications, networking, high-end computing, and ATE applications

PHOENIX, Ariz. – May 19, 2006 – Further expanding its high performance ECLinPS MAX™ family of clock and data management solutions, ON Semiconductor (Nasdaq: ONNN) today introduced the NB6L11S, and NB6N14S – two highly accurate, fully differential interface ICs. The devices are designed for precise clock management of telecommunications, networking, high-end computing, and automated test equipment (ATE) applications.

Both devices combine ON Semiconductor’s cutting edge bipolar capability with an LVDS compatible output structure, enabling them to interface directly with LVDS devices without sacrificing performance. In addition, both devices utilize the ON Semiconductor’s AnyLevelTM input structure, which provides seamless interfacing with LVPECL, CML, LVCMOS, LVTTL, or LVDS signals and offers true design flexibility.

The NB6L11S is a differential 1:2 Clock or Data translator and distribution device, with a maximum input clock frequency of greater than 2.0 gigahertz (GHz), and jitter of 500 femtoseconds (fs) typical. The device operates at Vcc of 2.5 volts (V), and is packaged in a Pb-free QFN-16. The NB6L11SMNR2G is priced at $3.50 per unit in 3,000 piece quantities.

The NB6N14S is a differential 1:4 Clock or Data translator and distribution device with a maximum input clock frequency of greater than 2.0 GHz, and jitter of 500 fs typical. The device operates at Vcc of 3.3 V, and is packaged in a Pb-free QFN-16. NB6L14SMNR2G is priced at $4.00 per unit in 3,000 piece quantities

For additional information or to order samples, visit https://www.onsemi.com. For additional information, contact Prescott Sakai at Prescott.Sakai@onsemi.com.

About ON Semiconductor
With its global logistics network and strong portfolio of power semiconductor devices, ON Semiconductor (Nasdaq: ONNN) is a preferred supplier of power solutions to engineers, purchasing professionals, distributors and contract manufacturers in the computer, cell phone, portable devices, automotive and industrial markets. For more information, please visit ON Semiconductor’s website at https://www.onsemi.com.

# # #

ON Semiconductor and the ON Semiconductor logo are registered trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the company references its website in this news release, such information on the website is not to be incorporated herein.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.