ON Semiconductor Expands Constant Current Regulator Offering for Solid State Lighting Systems

December 03, 2012

Fully integrated, feature-packed devices offer easy-to-use, high reliability, cost-effective alternative to discrete component approach in demanding AC off-line lighting applications











120 V Series of Constant Current Regulators

PHOENIX, Ariz. – Dec. 3, 2012 – ON Semiconductor (Nasdaq: ONNN), a premier supplier of high performance silicon solutions for energy efficient electronics, has introduced the new NSIC20xx series of linear Constant Current Regulators (CCR) designed for use in solid state lighting systems.

The new NSIC20XX series of CCRs offer a maximum voltage rating of 120 Volts (V), 3 Watts (W) and are capable of withstanding the high peak voltages of alternating current (AC) off-line HBLED lighting applications, including digital signage systems, lighting panels and decorative illumination. These new CCRs protect against the sudden surges that are commonplace in such lighting applications. Based on self-biased transistor (SBT) technology, the NSIC20XX series of devices are capable of current regulation over a very wide voltage range; while their negative temperature coefficient helps to protect the LEDs from thermal runaway at extreme voltage and current levels.

“As the demand for solid state lighting continues to grow, design engineers must be confident that the LEDs utilized are not in danger of being damaged by extreme temperatures or excessive current and that the long-term operation of the lighting system is assured,” said Dan Huettl, general manager and senior director of ON Semiconductor’s Small Signal products. “Featuring voltage surge suppression and negative temperature coefficient, the higher breakdown voltage capable, NSIC20XX series of CCRs provide the protection mechanisms needed to support the most demanding lighting application environments.”

The NSIC20XX series of CCRs provide a far simpler, more reliable and more cost-effective option of regulating the current of LEDs than conventional circuit design methodologies that rely on discrete and passive components. Because these devices do not require the specification of any external components, they can serve as either high or low side regulators, thus offering a streamlined solution that makes the development process more straight forward and maximizes design flexibility.

The NSIC2020BT3G, NSIC2030BT3G, NSIC2050BT3G have steady state current (IRegSS) capability of 20 milliamperes (mA), 30 mA and 50 mA, respectively. The devices turn on immediately and reach 45 percent regulation with an anode-cathode voltage (Vak) of just 0.5 volts (V) applied. The devices are designed to be thermally robust, supporting a junction temperature range of −55 °C to +175 °C and are UL94−V0 certified.

Packaging and Pricing
The NSIC2020BT3G, NSIC2030BT3G and NSIC2050BT3G are offered in a compact 2.20 mm x 3.56 mm x 4.32 mm, RoHS-compliant, SMB package and priced at $0.14 per unit in 10,000 unit quantities.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.