ON Semiconductor Expands Clock and Data Management Portfolio to Include New CML, LVDS, and ECL Interfaces

Share

The new functions and increased performance levels of the expanded clock and data management portfolio offer increased flexibility for high performance applications

PHOENIX, Ariz. – Feb. 15, 2006 – Expanding its high performance portfolio of clock and data management solutions, ON Semiconductor (Nasdaq: ONNN) today introduced the NB7L32M, NB4N11M, NB4N11S, and NB4L52 – highly accurate, fully differential interface ICs. The devices are designed for telecommunications, networking, high-end computing, and automated test equipment applications.

The NB7L32M is a divide by 2 Clock Divider with CML outputs that accepts differential LVPECL, CML, or LVDS inputs. With a maximum input clock frequency of 14 gigahertz (GHz) typical, and jitter of 130 femto-seconds (fs) typical, NB7L32M provides exceptional accuracy and speed for timing control applications. At this extended speed, the NB7L32M represents a new performance standard for Silicon Germanium based discrete clock and data management ICs. The device operates at Vcc of 2.5 volts (V) or 3.3 V, includes 50 ohm input termination resistors and is packaged in a space-efficient, Pb-free, 3 mm x 3 mm QFN-16. NB7L32MMNR2G is priced at $27.00 per unit in 3,000 unit quantities.

The NB4N11M is a 1:2 Clock Distribution chip with CML outputs, which accepts differential LVPECL, LVCMOS, LVTTL, CML, or LVDS inputs. NB4N11M has a maximum input clock frequency of > 2.5 GHz, and jitter of 1 picosecond (ps) typical. It features an innovative open collector CML output that facilitates a high speed interface between mixed voltage level ICs (1.8 V, 2.5 V and 3.3 V). This open collector output structure makes communication possible between a signal source operating at a different voltage than the destination IC. As Field Programmable Gate Arrays (FPGAs) and Application Specific ICs (ASICs) drive down toward lower voltage operation, the alternative to this device is usually level shifting using discrete components which add propagation delay, consume board space and increase costs. The NB4N11M requires no translation or level shifting. The device operates at Vcc of 3.3 V, and is packaged in a Pb-free 3 mm x 3 mm TSSOP-8. NB4N11MDTR2G is priced at $4.13 per unit in 2,500 unit quantities.

The NB4N11S is a 1:2 Clock Distribution chip with LVDS outputs that accept differential LVPECL, LVCMOS, LVTTL, CML, or LVDS inputs. Its introduction expands ON Semiconductors industry leading family of high performance LVDS interface devices. LVDS is a common interface for signaling in FPGAs and ASICs as an inexpensive differential option. However, traditional CMOS based LVDS devices lack the speed and precision necessary to delivery low jitter, tight timing signals. By marrying ON Semiconductor’s cutting edge bipolar capability with an LVDS compatible output structure, these LVDS devices offer better compatibility with mainstream ICs without sacrificing performance. This device has a maximum input clock frequency of > 2.0 GHz, and jitter of 500 fs typical. The device operates at Vcc of 3.3 V, and is packaged in a Pb-free QFN-16. NB4N11SMNR2G is priced at $3.50 per unit in 3,000 unit quantities.

The NB4L52 is a D Flip-Flop with LVPECL outputs, which accepts differential LVPECL, LVCMOS, LVTTL, CML, or LVDS inputs. NB4L52 has a maximum input clock frequency of > 4 GHz typical, and jitter of 1 ps typical. The NB4L52 is a pin for pin upgrade of the MC100EP52, adding support for a 2.5 V supply. The reduced voltage results in lower power consumption and the elimination of a power supply rail if it is otherwise unused. The device includes 50 ohm termination resistors, and is packaged in a Pb-free QFN-16. NB4L52MNR2G is priced at $5.00 per unit in 3,000 unit quantities.

For additional information or to order samples, visit https://www.onsemi.com. For additional information, contact Prescott Sakai at Prescott.Sakai@onsemi.com.

About ON Semiconductor
With its global logistics network and strong portfolio of power semiconductor devices, ON Semiconductor (Nasdaq: ONNN) is a preferred supplier of power solutions to engineers, purchasing professionals, distributors and contract manufacturers in the computer, cell phone, portable devices, automotive and industrial markets. For more information, please visit ON Semiconductor’s website at https://www.onsemi.com.

# # #

ON Semiconductor and the ON Semiconductor logo are registered trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the company references its website in this news release, such information on the website is not to be incorporated herein.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.