Two new integrated PoE-PD and DC-DC converter controllers support standard power 13 W applications and up to 40 W for extended high power applications

PHOENIX, Ariz. –September 29, 2008 - ON Semiconductor (Nasdaq: ONNN), a leading global supplier of high performance, energy efficient, silicon solutions has announced the availability of the NCP1080 and NCP1081, two new members of its Power over Ethernet (PoE) product family. The NCP1081 is the industry’s highest power integrated Power over Ethernet Powered Device (PoE-PD) supporting extended power ranges up to 40 watts (W) of regulated power delivered to the application load in a 2-pair configuration. Both devices fully support the IEEE 802.3af standard and the NCP1081 enables the latest approved IEEE 802.3at draft (D3.0) standard including two event physical layer classification. Typical applications targeted by NCP1080 and NCP1081 include VoIP phones, wireless access points, Industrial Ethernet devices, pan-tilt-zoom (PTZ) and dome IP cameras, RFID base stations, WiMax modems and could be considered for PC laptops.

Supplied in a TSSOP-EP20 package measuring just 4.4 mm x 6.5 mm, the pin-compatible NCP1080/1 combine in a single chip an enhanced PoE-PD interface and a highly efficient DC-DC converter controller. These highly integrated solutions reduce bill-of-materials (BOM) counts by up to 67 percent compared to other two chip solutions. The exceptional high power capabilities of the NCP1081 opens the door to a new class of products powered directly over Ethernet lines, eliminating the need for local power adaptors or power supplies and drastically reducing overall installation and maintenance costs.

The NCP1080/1 leverages ON Semiconductor’s automotive qualified high-voltage SmartPower process to provide superior cable ESD and surge protection levels compared to other integrated PD and DC-DC converter controllers. Low on-resistance (Ron) and extended temperature range allows the NCP1080/1 to achieve record power levels while operating in harsh environments.

“ON Semiconductor has an impressive track record in process, design and system innovations to solve our customers’ problems,” said Bob Kirk, ON Semiconductor marketing director of communications high-voltage Business Unit. “This enables us to identify and develop innovative products, such as high power PoE-PD, for a broad range of markets.”

The NCP1080/1 takes advantage of new and emerging power sourcing equipment (PSE). The NCP1080/1 devices support an adjustable under-voltage lock out mechanism, offer an integrated classification loop and allow for external programming of key parameters. Over-temperature protection and a two event physical layer classification indicator on the NCP1081 are standard features.

The devices' integrated DC-DC converter controllers facilitate the implementation of popular and proven single-ended power supply topologies such as fly-back, buck and forward converters and uses a control scheme based on peak current control. The controllers have all the features needed for a flexible, robust and highly efficient design, including programmable frequency, slope compensation and soft startup.

Pricing and Availability
The NCP1080/1 are currently available. Budgetary pricing for the NCP1080 is $1.45 USD and for the NCP1081 $1.80 USD for quantities of 1,000 units and above. NCP1081 and NCP1080 evaluation boards are available. For more information, please contact your local sales representative at www.onsemi.com.

About ON Semiconductor
With its global logistics network and strong product portfolio, ON Semiconductor (NASDAQ: ONNN) is a preferred supplier of high performance, energy efficient, silicon solutions to customers in the power supply, automotive, communication, computer, consumer, medical, industrial, mobile phone, and military/aerospace markets. The company’s broad portfolio includes power, analog, DSP, mixed-signal, advance logic, clock management and standard component devices. Global corporate headquarters are located in Phoenix, Arizona. The company operates a network of manufacturing facilities, sales offices and design centers in key markets throughout North America, Europe, and the Asia Pacific regions. For more information, visit https://www.onsemi.com.

# # #

ON Semiconductor and the ON Semiconductor logo are registered trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the company references its Web site in this news release, such information on the Web site is not to be incorporated herein.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.