ON Semiconductor Collaborates with ICs LLC to Develop Radiation Hardened ASICs for Military and Aerospace Applications

PHOENIX, Ariz. – Nov. 18, 2014 –

Share

Access to comprehensive RHBD IP adds further dimension to existing ASIC offering, allowing wider range of high reliability applications to be addressed















PHOENIX, Ariz. – Nov. 18, 2014 – ON Semiconductor (Nasdaq: ONNN), driving energy efficiency innovations, has entered into a licensing/development agreement with ICs LLC in order to bring application specific integrated circuits (ASICs) to market which are resilient to radiation effects. Radiation hardened by design (RHBD) ASICs created through this agreement will be based upon ON Semiconductor’s ONC110 110 nanometer (nm) process for ASIC designs and production. The introduction of RHBD ASICs extends the company’s military and aerospace offering that includes ITAR compliance, DMEA Trusted Supplier accreditation and DO-254 support.

Radiation testing has exhibited strong single event upset and single event latch-up immunity performance with onset linear energy transfers (LETs) in excess of 100 MeVcm2/mg for the ASICs and double-bit upset immunity of 40 MeVcm2/mg for the dual port SRAM. In addition, a novel RHBD flip-flop architecture has been introduced, referred to as Self Restoring Logic (SRL). The SRL flip flops have shown hardness resilience to single event effects at frequencies of up to 700 megahertz (MHz). Principal targets for these new RHBD ICs will be high reliability (hi-rel) applications, such as space exploration, satellite communication and surveillance, avionics, unmanned aerial vehicles (UAVs), commercial aircraft, nuclear energy, particle physics research and military equipment,

“The mitigation of radiation effects is becoming an increasingly serious issue as the industry moves to smaller semiconductor process architectures,” explained Dr. Joe Feeley, CEO at ICs LLC. “Legacy RHBD solutions for SEU immunity do not provide adequate protection for high speed circuits, while SRL does. ON Semiconductor is uniquely able to provide a solution to this important problem and enable customers to produce fault tolerant ASICs for important real time applications.”

Vince Hopkin, vice president, Military/Aerospace, Digital and Custom Foundry at ON Semiconductor added: “Thanks to this far-reaching agreement with ICs LLC, ON Semiconductor can support our customers’ demands for ASICs requiring a greater number of logic gates and smaller process technologies while also safeguarding extensively against failures caused by exposure to radiation. When combined with our Trusted source status and our capability to provide highly secure development flows, the addition of RHBD products to our portfolio will mean we are extremely well positioned to serve a broad spectrum of aerospace, military, and space programs, where the need for data and IP integrity is of paramount importance.”

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.