ON Semiconductor Adds New Clock and Data Driver ICs to its Family of Clock Management Products

PHOENIX, Ariz. – Jan. 26, 2010 –

Share

Low voltage drivers provide datacom and telecom equipment manufacturers with increased data rates and higher levels of signal integrity

ON Semiconductor Adds New Clock and Data Driver ICs to its Family of Clock Management ProductsPHOENIX, Ariz. – Jan. 26, 2010 – ON Semiconductor (Nasdaq: ONNN), a premier supplier of high performance, energy efficient silicon solutions for greener electronics, today announced an expansion of its family of clock drivers, with the release of the NB7L585, NB7L585R, NB7V585M and NB7V586M differential 2:1 mux input to 1:6 devices, and the NB6HQ14M and NB7HQ14M 1:4 fanout clock/data drivers with equalization.  

The NB6HQ14M and NB7HQ14M integrate a selectable equalizer receiver into a high performance differential 1:4 CML clock driver. When placed in series with a data path operating at up to 6.5 gigabits per second (Gbps) or 10 Gbps the inputs will compensate the degraded signal and output four identical CML copies of the original input signal. The serial data rate is thereby increased by reducing Inter-Symbol Interference (ISI) caused by losses in the copper interconnect or long cables.

The NB7L585, NB7L585R, NB7V585M, and NB7V586M are the newest members of the Gigacomm™ family representing a new 2:1:6 function integrating a 2:1 mux with a 1:6 fanout buffer.  The NB7L585 and NB7L585R are 2.5 V / 3.3 V devices with either Low Voltage Positive Emitter Coupled Logic (LVPECL) output or Reduced Swing Emitter Coupled Logic (RSECL) output of 400 millivolt (mV) peak-to-peak, respectively. The NB7L585 operates up to 5 gigahertz (GHz) or 8 Gbps and the NB7L585R operates up to 7 GHz or 10 Gbps.

The NB7V585M is an ultra low voltage device operating from a 1.8 V / 2.5 V power supply. The NB7V586M operates from an ultra low 1.8 V supply and offers the 6 outputs configured as three banks of two differential pairs. Each bank of outputs has the flexibility to be powered by any combination of either 1.8 V or 1.2 V supplies. Both devices operate up to clock/data rates of 6 GHz / 10 Gbps.

The specifications achieved by these clock drivers make them highly suited to use in SONET, Gigabit Ethernet, Fiber Channel, backplane and other clock/data distribution applications. The ambient operating temperature of each of these devices covers −40 °C to +85 °C.

“The system designs for telecom switches, servers and routers are under pressure to support ever increasing clock and data interfaces and voltage levels without compromising on the signal quality,” said Prescott Sakai, director, clock and data management business unit, ON Semiconductor. “The company’s new clock drivers enable new integrated functions with equalization features that support various interfaces and low voltage level options. These devices maintain higher signal integrity at data rates that the competing suppliers simply cannot match.”

Packaging and Pricing
Pricing for the NB7L585, NB7L585R, NB7V585M, NB7V586M, NB6HQ14M and NB7HQ14M start from $5.25 in 1,000 unit quantities. They are all offered in low profile 3 mm x 3 mm 16-pin or 5 mm x 5 mm 32-pin Pb-free QFN packages. Samples are available now.

For more information, please visit https://www.onsemi.com.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.

If you are a member of the press and are interested in receiving onsemi press releases via email, please complete the form below.

* Full Name

* Email

* Media you represent

* Press Category

*Required fields

Choose your prefered language. You can choose more than one.