New Multi-Output LDO Regulator From Semiconductor Components Group Is Complete Power Management Control For Portable Communication Devices

Share

Phoenix, Arizona - August 2, 1999 -- Portable battery powered communication systems can now be designed smaller, lighter and quieter thanks to a new highly integrated multi-output, ultra-low noise, low dropout (LDO) voltage regulator introduced by Motorola's Semiconductor Components Group today. The unit comes packaged in a 32-pin miniature package.

This new regulator is a comprehensive power management solution designed specifically for applications such as TDMA and GSM phones where the transmitter is continuously switched ON and OFF. It can also be used in other wireless cellular phones, Personal Digital Assistants (PDAs), telephone handsets and two-way radios.

The MC33283 offers up to 7 LDO regulators and a regulated step-up charge pump converter in one miniature package. All of the internal regulators supply voltage to all elements of the end product and can be independently switched ON and OFF. By having up to 7 independent regulators in one package, extra components can be eliminated in designs that require more than one regulator. This allows the voltage distribution of the entire product to be managed within one device thereby reducing the number of interconnecting printed circuit board PCB tracks used and significantly minimizes the potential problem of stray inductances. Consequently, the size of the PCB is also decreased.

"We realize that each portable communication system has its own unique architecture," comments Scott Delaney, Director of Marketing for Semiconductor Components Group. "What the development of the MC33283 demonstrates is Motorola's capability and eagerness to collaborate with customers to design application specific voltage regulators of various integration schemes".

Onboard the MC33283 resides an internal charge pump that can supply the flash memory or a Subscriber Identification Module (SIM) card. Yet, the device offers excellent overall noise characteristics of only 40=B5V RMS @ nominal output current levels from 10kHz to 100kHz making it an ideal circuit for designs where noise is a critical consideration.

Furthermore, it is equipped with a Power On Reset feature as well as an Undervoltage Lock Out protection feature that increases the reliability and ruggedness of the final design. Additionally, it supplies voltage to the Baseband processor and other logic, analog and RF devices which make up the final system.

The MC33283 is housed in a miniature TQFP-32 pin package that simplifies PCB layout. Samples and production quantities are now available with pricing of $1.60 in 10K quantities.

About ON Semiconductor
ON Semiconductor, formerly a division of Motorola, is the world's leading supplier of analog ICs, logic ICs and discrete semiconductors with shipments of 18 billion units in 1999. Sales in 1998 exceeded $1.5 billion (pro forma). ON Semiconductor's products include integrated circuits for high-bandwidth data applications, analog ICs for power management, as well as low-voltage power transistors and the most complete discrete semiconductor portfolio in a variety of surface mount and standard packages. These semiconductor components provide the connectivity for digital electronic products. ON Semiconductor is the trade name of Semiconductor Components Industries, LLC. https://onsemi.com

# # #

Motorola is a registered trademark of Motorola, Inc.

Photo available through Editorial contact.

For more information:

Yinka Massally
Public Relations Manager
ON Semiconductor
602-244-6398
Laurent Jenck
ON Semiconductor
602-244-4266

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.