PHOENIX, Ariz. – March 9, 2020 –

Share

Multi-channel platform with Bluetooth® Low Energy and PoE capability addresses energy efficiency and convenience

PHOENIX, Ariz. – March 9, 2020 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, has introduced the Connected Lighting Platform, leveraging the company's expertise in Power over Ethernet (PoE) and ultra-low-power Bluetooth® Low Energy connectivity, along with AC/DC and DC/DC power conversion design.

The prototyping platform enables engineering teams to explore and innovate in the connected lighting sector, where light fittings become part of the Internet of Things (IoT). The Connected Lighting Platform features multiple forms of connectivity for LED control, including secured Bluetooth Low Energy, provided by the RSL10 SIP, and Power over Ethernet. It offers up to 90 Watts output power and provides two independent channels, each able to supply and control up to 16 LEDs. The high-efficiency modular platform also enables the development of battery-less LED lighting applications when used together with the Energy Harvesting Bluetooth Low Energy Switch.

Comprehensive software tools support the Connected Lighting Platform, including an Integrated Development Environment (IDE), various use-cases, and mobile apps. The platform allows LEDs to be controlled wirelessly using the RSL10 Sense and Control app (available for iOS® and Google Play™), or through a web client. Using the RSL10 FOTA app (iOS®,Google Play™) firmware updates can be easily sent after the application has been deployed.

Alongside the platform, ON Semiconductor has also developed a PoE module for high-power, wired connectivity. Based on the IEEE 802.3bt compliant NCP1096 interface controller, the module extends the platform to provide access to 90 W of power that can now be delivered through an Ethernet cable.

Commenting on the introduction of the Connected Lighting Platform, Wiren Perera, who heads IoT strategy at ON Semiconductor, said: “Lighting is one of the most significant consumers of energy across the globe. By combining flexibility, wireless control, and energy efficiency, the Connected Lighting Platform allows manufacturers to drastically reduce their energy consumption while providing greater user convenience."

The Connected Lighting Platform is available now through local ON Semiconductor sales support representatives and authorized distributors.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.