Our knowledge base of frequently asked questions (FAQs) contains answers to questions from designers like you. Ask our experts a question of your own. Or, browse these FAQs by category or search key words.
Where
Question
Answer
contains
AND
OR
Question
Answer
also contains
Product
Questions
Views
AR0237CSSC12SPRA0-DR-ECR
We want to use your evaluation kit AR0237CSSC00SUEAD3-GEVK with a Linux system. Will the camera be recognized from a Linux as a camera device using video4 Linux?
171
NCP59749MN2ADJTBG
Do you have a voltage regulator that will support 5V input and regulate to 3.3V and 2-3A . It nust have the ability to limit inrush current.
389
NCV8450ASTT3G
For NCV8450A, do you have EMC test including ESD? Also, could you advise on the following: The power supply is 16V, the output has a pull up resistor about 3.2Kohm. If we add a voltage about 7.6v to Vout, could it damage NCV8450A?
664
NCV7240DPR2G
Can you provide the shear stress test results for NCV7240? This is required for AEC-Q100 qualification.
959
ESD11B5.0ST5G
Can you please explain the difference between ESD11B5.0ST5G and SSESD11B5.0ST5G?
793
AMIS42770ICAW1G
Can you clarify the functionality of the Vref pin on the AMIS42770
1337
NUP2105LT3G
I have a question related to Rt and Ct found in fig. 12 of AND8253/D written by Jim Lepkowski. I need to provide surge suppression for a CAN transceiver in a system that will be subjected to power short-circuit tests. In these tests all external I/O are shorted to a 32V source for one minute. An unprotected NUP2105L would breakdown, conduct and burnout during this test. Fig. 12 of AND8253/D shows a way to avoid this problem. How do I calculate the values of Rt and Ct? Should Rt be a "pulse withstanding" type? How much power can I let the NUP2105L dissipate safely? What would be a good value for Ct? Is there anything special about Ct?
1898
GENERAL
Can the P6SMB36CAT3G replace SZP6SMB36CAT3G in an automotive application?
2011
AMIS42700WCGA4H
What is the difference between the AMIS42700 and AMIS42770?
2151
AMIS42700WCGA4H
Can the AMIS-42700 filter CAN messages between the two buses on the chip between AMIS-42700 chips?
1961
CS3361YDR14G
I am looking for a 3-phase rectifier / N-FET controller for an alternator application.
1936
GENERAL
I am looking for a component which can provide enough protection against Pulse 5b described in ISO16750-2:2012, with the parameter td=400ms, Us=87V, Ri=0.5ohm. Do you have a recommendation?
2146
NCV7341D20G
What is the maximum power dissipation of the NCV7341D20G? Also, does the current consumption of the transciever vary with the data rate?
2522
GENERAL
Does ON Semiconductor offer automotive rated and certified products?
2778
Question
Applications
Select ...
Automotive
Circuit Protection
Computing and Peripherals
Consumer
Corporate
Industrial
LED Lighting
Medical
Military & Aerospace
Motor Control
Networking and Telecommunications
Portable and Wireless
Power Supply
Product