Our Ask An Expert knowledge base contains answers to questions from designers like you. Browse the knowledge base by category or search key words. Not seeing what you need? Ask An Expert a question of your own.
Hi, My earlier question was "We are using this device P/N: CAT4240TD-GT3 for one of LCD boost operation with 24V Vout. We need to understand how this device can used for 9.3V PWM out with 120 mA with Vin = 5V "..to add further..we are using PWM signal input to SHDN Pin to control PWM output for dimming appliction. VIN is at 5V. Are we able to get 9.3V @ 120 mA if we get the value of Rs = 2.5Ohm and L= 26 uH..please confirm..
Yes, as I have explained in previous post.LED brightness dimming can be done by applying a PWM signal to the SHDN input. The LED current is repetitively turned on and off, so that the average current is proportional to the duty cycle. A 100% duty cycle, with SHDN always high, corresponds to the LEDs at nominal current. The recommended PWM frequency range is from 100 Hz to 2 kHz and the maximum voltage on SHDN pin is 7V.
Answered by: ON Semiconductor
2013-01-23 14:42:38.946