feedback
Rate this webpage

Need
Support?


Ask An Expert

Our Ask An Expert knowledge base contains answers to questions from designers like you. Browse the knowledge base by category or search key words. Not seeing what you need? Ask An Expert a question of your own.
All   >>  LED Lighting   >>   Mobile Applications   >>   Questions
 

Subject: Need support on "Sequential Read" Description: Hi, I am trying to write and read to EEPROM. (Processor: freescale IMX6Q) I can read single byte successfully. Also, when i try to read EEPROM using Sequential Read (Multibyte read), i can read data bytes from 0 to 255, 256 to 511 etc (in multiple of 255 , ie: 0xFF) correctly. However, If i try read bytes: 0 to 511, i get correct value from 0 to 255, but wrong values from 256 to 511. What is the reason? and how i can correct it? Please reply asap. Thanks. Regards, Keshava G N Member - Technical, iWave Systems, Bangalore, India An additional information: Part number: CAT24AA16TDI-GT3 VCC = 1.8 v Clock freq = 400kHz I read/write happening correctly. However, while using sequential read, in the boundaries of : FFh (ie: 255 in decimal) address (example: read values from 250 to 260), I get correct values only from 250 to 255, but get only FF from 256 to 260. Please help to solve the issue.

A1:Would you please provide part number (EEPROM) are you referring to and more details about application conditions: VCC, Clock freq, etc? A2: For this particular case, I have to check with you how you address the part when Reading in Sequential mode. Per the device data sheet, the Memory space address requires 11 Address bits: : 8 bits are sent during the “ADDRESS byte” and 3 bits are part of the “Slave Address Byte” . - So we need to make sure you have a correct combination for the a10, a9, a8 from the Slave Address byte. You need to start with a10, a9, a8 bits = 0, 0, 0. The CAT24AA16 should be able to continue sending data out up to the end of Last Addr Byte = 0x7FF and when reaches the last address it will wrap around to zero (during Sequential Read). - I cannot see any reason do not work this way, except inside there is a different memory size: maybe it is not a 16Kb memory !? Can you provide Top package marking, Date Code..? - Please provide also details like: customer name and application, if NEW design ..? Have you used our part before ..? How many parts are behaving in this way ..? etc .. Answered by:
ON Semiconductor
2013-02-12 09:34:32.089