feedback
Rate this webpage

Need
Support?


Ask An Expert

Our Ask An Expert knowledge base contains answers to questions from designers like you. Browse the knowledge base by category or search key words. Not seeing what you need? Ask An Expert a question of your own.
All   >>  LED Lighting   >>   Automotive Lighting Applications   >>   Questions
 

From your note, I understand I have to place a 1meg ohm resistor in series with the three units which are in parallel. That high of a resistance will not let the 1000ma pass will it? Going across a straight 12v, a 1meg resistor will only allow 12micro amps. Maybe I misunderstood the note. Can you clarify? -------------------------------------------------------------------------------- From: onhelp@onsemi.com To: dsdrewyor@comcast.net Sent: Monday, February 2, 2015 6:14:26 PM Subject: Ask An Expert Notification Your question: I have an LED that has a Fv of 3.3v and up to 1000ma drive requirement. My drive source is a PWM signal at 12vdc up to the 1000ma max. What can I use to limit the drive voltage to the LED while still getting the current I need? I have used dropping resistors in the past, but these would be very large resistors. Thanks Dave has been answered: You can use our NSI50350AS LED Driver, Constant Current Regulator, 350 mA, 50 V and connect three of them parallel with 1 m Ohm resistor in series. This configuration will limit your LED current to 1 Amp. If you have more questions please visit: AskAnExpert application Kind regards, ON Semiconductor

Hello, Series resistor value should read 1 milliohm not Mega ohm. Let me know if you have any other questions. Answered by:
ON Semiconductor
2015-02-16 10:03:38.18