Our Ask An Expert knowledge base contains answers to questions from designers like you. Browse the knowledge base by category or search key words. Not seeing what you need? Ask An Expert a question of your own.
Hi, I designed a POE+ PD device and tested it. it works fine with POE+ PSE, But when I connect it to a POE PSE, then also it works. The PSE should detect this as POE+ and shouldn't source power to PD. Rclass is R29, and resistor value used is 30.9ohms.
Class 4 is also defined in 802.3af, where it will deliver 13W. The difference has to be detected by the application using the nClass_at pin, which will be pulled down only when the PD is connected to an 802.3at PSE. The application can then decide to disconnect everything, or start up in a limited mode that consumes less power.
Answered by: ON Semiconductor
2013-04-17 08:27:45.426