feedback
Rate this webpage

Need
Support?


Ask An Expert

Our Ask An Expert knowledge base contains answers to questions from designers like you. Browse the knowledge base by category or search key words. Not seeing what you need? Ask An Expert a question of your own.
All   >>  Energy Efficiency   >>   Power Supplies   >>   Questions
 

I want to use your NCV8664 regulator to power a linear Hall sensor. We need to program this device after it is packaged. Can I raise the regulated 5 V output to 8 Volts without damaging the regulator? Thank you Norm Poirier

If your input is Vin> 8V and V out =8V LDO is turned off .No current is flowing from the input to the output. Current starts flowing if Vin is lower than 7.3V and output transistor is reverse biased. Higher the difference between V out – V in higher the reverse current will be. Reverse current is not very high and unless your junction temperature is under 150C there should be no problem to operate NCV8664ST50T3G in reverse. Let me know if you have any other questions. Answered by:
ON Semiconductor
2013-04-05 07:18:30.199