feedback
Rate this webpage

Need
Support?


Ask An Expert

Our Ask An Expert knowledge base contains answers to questions from designers like you. Browse the knowledge base by category or search key words. Not seeing what you need? Ask An Expert a question of your own.
All   >>  Energy Efficiency   >>   Power Supplies   >>   Questions
 

Good morning. I have looked through the data sheet and the Reference Manual, SOLDERRM/D, but cannot find information about component terminal finish. Therefore please could you let me know what is the terminal finish for Diode BZX84CxxxLT1G. If it is Matte Tin, is it annealled at 150C. Is there a Nickle under plate etc? Is there a web link that will fully identify terminal finish for all of your components? Regards John

Material content details are visible via material composition link at: http://www.onsemi.com/PowerSolutions/MaterialComposition.do?searchParts=BZX84C10L In this case for the diode BZX84CxxxLT1G finish plating is 100% matte tin. Changing the lead plating material to 100% matte Sn (tin) from SnPb raises industry concerns about tin whisker growth. ON Semiconductor has implemented the following mitigation strategies to minimize the occurrence of tin whiskers. • Increased the plating thickness from 5 µ m to 7.5 µ m minimum; 10 um nominal. • Implemented a post - plate anneal of 150 ° C for 1 hour within 24 hours of plating • Implemented strict plating process controls For more details please see tin whiskers strategies at: http://www.onsemi.com/PowerSolutions/content.do?id=17097 Answered by:
ON Semiconductor
2013-02-01 09:33:45.073