Our Ask An Expert knowledge base contains answers to questions from designers like you. Browse the knowledge base by category or search key words. Not seeing what you need? Ask An Expert a question of your own.
Hello,
I'm interesting by the CAT4104 for my new design. In the datasheet, I read this :
1 - "Accurate linear dimming is compatible with PWM frequencies from 100 Hz to 5 kHz for PWM duty cycle down to 1%.".
2 - Maximum EN/PWM high time = 5us
Does it mean that :
- if my PWM frequency is 5kHz, the minimum duty cycle is 1% but if my PWM frequency is 1kHz, the minimum duty cycle can be 0.2% ?
OR
- the minimum duty cycle is 1% from 100Hz to 5kHz ?
Thank you in advance.
The linearity is accurate down to 1% for the PWM. Notice at 5 us with 5 kHz PWM the duty cycle is 2.5% but the LEDs are effectively at 1% brightness when accounting for rise/fall times. This is at the most extreme operation where it’s already a bit non-linear.
You can run any timing as long as the THI and TLO specifications are obeyed, but the relationship may be non-linear below 1% duty cycle.
Answered by: ON Semiconductor
2015-02-18 13:20:29.683