Our Ask An Expert knowledge base contains answers to questions from designers like you. Browse the knowledge base by category or search key words. Not seeing what you need? Ask An Expert a question of your own.
Hi. I am going to use MC34063 for Boost Step up converter. I have used You calculator and it Works OK, bur here are my quistion: I need to have minimum 20V output, and the input cam be from 8-34V DC, will it be OK to apply higher input than output? I know that to output will follow input minus diode voltage, and that ik OK. It shall deliever supply for a laser sensor, and the laser sensor need 18-33V for working, so it OK that the voltage increase, but do it harm the MC34063?? I am aware, that I can put a PNP transistor on, so that the voltage alwayes will be 20B , but I don't need taht, all I need is that there alwayes is minimum 18V for sensor, therefore I choose 20V. Quistion2: Is it possibel to control ON/OFF of the converter? Mayve with a diode catode to Vref, and then apply 5V on anode of diode, will that be OK? Thank Yoy very much Per Haastrup Denmark
A complete step−up/down switching regulator design example is shown in Figure 18 theory and applications of the MC34063.
There is also possibility for ON/OFF control of the converter. Please refer to our application note AND8298 related to the NCP3065 application examples are on the page 3.
Answered by: ON Semiconductor
2014-08-20 13:33:45.972