Our Ask An Expert knowledge base contains answers to questions from designers like you. Browse the knowledge base by category or search key words. Not seeing what you need? Ask An Expert a question of your own.
We are using MC33035 for controlling the BLDC motor. Currently we are connecting a Potentiometer between reference output and Error non-inverting input.We like to control the Speed using the PWM of micrcontroller. Let me know how we can do this.
You did not specify the desired precision of the speed-set function. So I am going to assume, moderate? precision, not high-precision, since he is now using a potentiometer. Refer to Figure 39 on page 20 of the MC33035 datasheet. The Error Amp is part of a control loop that compares two DC voltages (representing set-speed and actual speed), and outputs a DC voltage to the input of the PWM comparator. The set-speed input must therefore be DC. The requirement therefore becomes how to generate a DC voltage that is proportional to a PWM signal duty cycle. To describe the functional requirement as a simple table: = duty cycle ==== output V ==================== == 0% ========= 0V == == 100% ====== Vreg (MC33035 Pin 8) == 50% ======= Vreg / 2 Step one is to make the PWM signal vary between 0 and Vreg, independent of actual amplitude. This could be a comparator, single transistor amplifier, or operational amplifier (all of these would have Vcc / Vdd connected to Vreg, thus setting the maximum output voltage at Vreg. Step two to is to average the output, this could be a simple RC integrator, or better, an inverting op amp configured with an input resistor to set a charge current, and a parallel-connected RC between output and (inverting) input. The non-inverting input would be connected to Vreg. The output is connected to Pin 11 of the MC33035. A dual op-amp could be used to manage both functions. It must be single-supply ?rail-to-rail? type because common-mode input range is 0 to Vreg, and the amplifiers are powered by Vreg.
Answered by: ON Semiconductor
2011-06-15 17:58:36.0