Our Ask An Expert knowledge base contains answers to questions from designers like you. Browse the knowledge base by category or search key words. Not seeing what you need? Ask An Expert a question of your own.
Dear Sir/Madam,
i am a student and i am in the process of my thesis diploma. As part of it, i need a voltage regulator that will take as input 5V and will give as output 3V. Unfortunately i have searched everywhere and the only ones i find are those who give as output 3.3V.
After a good look at your site, i saw that you have some DC/DC converters like the NCP1402 that could do the job, but i am not so sure. The reason i need the specific regulator is because my power source is at 5Volts and for the needs of my circuit, i need at a specific IC a 3Volts Vref.
Do you think that you have something that could help me?
Thank you in advance,
Pantelis
Based on the information provided we can suggest LM317. The LM317 is an adjustable 3−terminal positive voltage regulator capable of supplying in excess of 1.5 A over an output voltage range of 1.2 V to 37 V.
Answered by: ON Semiconductor
2013-08-19 15:26:26.843