<?xml version="1.0" encoding="UTF-8" standalone="yes"?>
<MainDeclaration version="2.0" xmlns="http://webstds.ipc.org/175x/2.0">
    <BusinessInfo mode="Distribute">
        <Response comment="Generated by OnSemi.com" fieldLock="false" date="2026-05-31">
            <Authorizer name="Product-Env-Stewards">
                <Email address="Product-Env-Stewards@onsemi.com"/>
                <Phone number="NA"/>
            </Authorizer>
            <SupplyCompany name="ON SEMICONDUCTOR">
                <CompanyID identity="" authority=""/>
            </SupplyCompany>
            <Contact name="Product-Env-Stewards">
                <Email address="Product-Env-Stewards@onsemi.com"/>
                <Phone number="NA"/>
            </Contact>
        </Response>
        <Declaration legalType="Custom" supplierAcceptance="true" legalDef="Please indicate whether any homogeneous material (as defined by the RoHS Directive, 2015/863/EU amending RoHS Directive 2011/65/EU and implemented by the laws of the European Union member states) of the part identified on this form contains lead, mercury, cadmium, hexavalentchromium, polybrominated biphenyls and/or polybrominated diphenyl ethers (each a “RoHS restricted substance”) in excess of the applicable quantity limit identified above. If a homogeneous material within the part contains a RoHS restricted substance inexcess of an applicable quantity limit, please indicate below which, if any, RoHS exemption you believe may apply. If the part is an assembly with lower level components, the declaration shall encompass all such components.Supplier certifies that it gathered the information it provides in this form using appropriate methods to ensure its accuracy and that such information is true and correct to the best of its knowledge and belief, as of the date that Supplier completes this form.Supplier acknowledges that Company will rely on this certification in determining the compliance of its products with European Union member state laws that implement the RoHS Directive. Company acknowledges that Supplier may have relied on informationprovided by others in completing this form, and that Supplier may not have independently verified such information. However, in situations where Supplier has not independently verified information provided by others, Supplier agrees that, at a minimum, itssuppliers have provided certifications regarding their contributions to the part, and those certifications are at least as comprehensive as the certification in this paragraph.If the Company and the Supplier enter into a written agreement with respect to the identified part,the terms and conditions of that agreement, including any warranty rights and/or remedies provided as part of that agreement, will be the sole and exclusivesource of the Supplier’s liability and the Company’s remedies for issues that arise regar" uncertaintyStatement=""/>
    </BusinessInfo>
    <Include>
        <Sectional name="MaterialInfo">
            <SubSectional name="A"/>
            <SubSectional name="D"/>
        </Sectional>
    </Include>
    <Product unitType="Each" numberOfInstances="1">
        <ProductID itemNumber="PCFA86561F" manufacturingSite="PBB" version="1">
            <Amount value="5.73000000" UOM="mg"/>
        </ProductID>
        <MaterialInfo>
            <ExemptionList/>
            <QueryList identity="EUROHS-0508">
                <Query response="true" statement="Product Meets EU RoHS Requirements Without Any Exemptions"/>
                <Query response="false" statement="Product Meets EU RoHS Requirements Except Lead in Solder and This Usage May Qualify Under the Lead in Solder ''7b'' Exemption (other selected exemptions may apply)"/>
                <Query response="false" statement="Product Meets EU RoHS Requirements by Application of the Selected Exemption(s)"/>
                <Query response="false" statement="Product Fails to Meet EU RoHS Requirements"/>
                <Query response="false" statement="Product is Unknown/Obsolete, No Information is Available"/>
            </QueryList>
            <HomogeneousMaterialList>
                <HomogeneousMaterial name="Die">
                    <Amount value="5.73000000" UOM="mg"/>
                    <SubstanceCategoryList>
                        <SubstanceCategoryListID identity="Supplier" authority="Supplier"/>
                        <SubstanceCategory name="NA">
                            <Substance name="Silicon (Si)">
<SubstanceID identity="7440-21-3" authority="CAS"/>
<Amount value="5.73000000" UOM="mg"/>
                            </Substance>
                        </SubstanceCategory>
                    </SubstanceCategoryList>
                </HomogeneousMaterial>
            </HomogeneousMaterialList>
        </MaterialInfo>
    </Product>
</MainDeclaration>