Next-Generation onsemi 1200 V EliteSiC M3S Devices

SCOTTSDALE, Ariz. – May 9, 2023 – onsemi (Nasdaq: ON), a leader in intelligent power and sensing technologies, today announced the release of the latest generation of 1200 V EliteSiC silicon carbide (SiC) M3S devices, which enable power electronics designers to achieve best-in-class efficiency and lower system cost.


ON Semiconductor Announces New Automotive Traction Inverters

Consumer Electronics Show (CES) – Venetian 3302 – LAS VEGAS, NV. – 16 December 2019 – ON Semiconductor (NASDAQ: ON), driving energy efficient innovations, has released the first two devices from its new VE-Trac™ family of power modules for high voltage automotive traction inverters. These two power integrated module (PIM) devices bring best-in-class electrical and thermal performance while providing scalability and automotive reliability to the rapidly growing market for traction inverters.

Related Product:  NVG800A75L4DSC 


New Family of Multi-Chip Module PWM Buck Regulators

PHOENIX, Ariz. – June 25, 2018 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, has announced the release of three new highly-efficient mid-voltage PWM buck converters.

Download: JPG - 390.1kB  


FDFM8811 Wins Top 10 Power Product Award 2017 in China

BEIJING, China – September 15, 2017 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, today announced that its industry-first FDMF8811 100 V bridge power stage module for half-bridge and full-bridge DC-DC converters has won a Top 10 Power Product Award 2017. Organized by Electronic Products China and 21ic.com, the awards program is a highly recognized benchmark in identifying innovative products for the electronics industry.

Download: JPG - 49.7kB  


Industry’s First 100V Bridge Power Stage Module

APEC 2017 – Booth #1001 - TAMPA, FL – March 27, 2017 – – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, has launched the FDMF8811, the industry's first 100 V Bridge Power Stage modulefor half-bridge and full-bridge isolated dc-dc converters. The 25 A-rated device integrates a 120 V driver IC, a bootstrap diode, and two highly efficient power MOSFETs in a PQFN-36 package.

Download: JPG - 355.4kB  


New Portfolio of DDR Termination Regulators
New Portfolio of DDR Termination Regulators

ON Semiconductor (Nasdaq: ON), driving energy efficiency innovations, has further strengthened its low drop-out (LDO) linear voltage regulator portfolio with the introduction a series of new high performance devices to support double data rate (DDR) memory. The NCP51200, NCP51510, and NCP51199 feature built in Power MOSFETS and are targeted at a wide variety of applications in the computing, data networking, industrial and handheld consumer markets for specific applications such as SDRAM DIMM memories, servers, routers, smartphones, tablet computer platforms, set top boxes, smart TVs, printers, and PC/laptop motherboards. AEC−Q100 qualified versions are also available for automotive applications including embedded GPS mapping systems, Infotainment, and Wifi and Bluetooth communications.

Download: JPG - 638.2kB  JPG - 83.2kB  

Related Products:  NCP51510  NCP51400  NCP51199  NCP51200 


 NCV896530 DC-DC buck converter image
New Automotive Grade Power Management ICs

PHOENIX, Ariz. – Oct. 28, 2013 – ON Semiconductor (Nasdaq: ONNN), driving energy efficient innovations, has introduced two new AEC Qualified ICs which, thanks to their wide input voltage range and extensive operational temperature range, are highly optimized for automotive powertrain and in-cabin deployment.

Download: JPG - 615.0kB  JPG - 685.7kB  

Related Products:  NCV896530  NCV8876 


ON Semiconductor Addresses Modern Power Design Challenges
ON Semiconductor Addresses Modern Power Design Challenges

Cutting-edge digital AC-DC PWM controllers, motor drivers and IGBTs to be demonstrated by the company at industry’s premier power electronics show

Applied Power Electronics Conference (APEC) – LONG BEACH, Calif. – March 18, 2013 – ON Semiconductor (Nasdaq: ONNN), driving innovation in energy efficiency, will showcase its latest power efficient product advances at APEC 2013, March 17 - 21, 2013, in Long Beach, California. The new devices are designed for boosting performance and simplifying the design of offline power supplies, AC lighting infrastructure and motor control systems.

Download: JPG - 387.6kB  

Related Product:  NCP1937 


The NCP6338 is an integrated DC-DC Converter for Multi-Core Processors
Integrated DC-DC Converter for Multi-Core Processors

PHOENIX, Ariz. – Nov. 5, 2012 – –– ON Semiconductor (Nasdaq: ONNN), a premier supplier of high performance silicon solutions for energy efficient electronics, addresses the growing need for higher power densities in portable consumer electronics designs with the introduction of the , a configurable, 6 Ampere (A) step down DC-DC converter integrated circuit (IC).

Download: JPG - 749.2kB  

Related Product:  NCP6338 


Power Management ICs Optimized for Portable Electronics
Power Management ICs Optimized for Portable Electronics

ON Semiconductor (Nasdaq: ONNN), a premier supplier of high performance silicon solutions for energy efficient electronics, has introduced two new power management integrated circuits (PMICs) optimized for battery powered systems such as smartphones, tablets, digital cameras, GPS systems and other portable electronics. Utilizing the latest power management techniques, the NCP6924 and NCP6914 optimize system efficiency and save battery life.

Download: JPG - 697.2kB  

Related Products:  NCP6914  NCP6924 


New Fully Integrated Li-Ion Battery Charger
Fully Integrated Li-Ion Battery Charger

ON Semiconductor, a premier supplier of high performance silicon solutions for energy efficient electronics, has introduced a fully programmable Lithium- Ion (Li-Ion) switching battery charger optimized for power efficiency in smart phones, tablets and other handheld devices. The NCP1851 significantly reduces charge time, increases battery life and includes advanced startup features.

Download: JPG - 803.6kB  

Related Product:  NCP1851 


Integrated Switching Buck Regulator
ON Semiconductor Introduces Integrated Switching Buck Regulators with Industry Leading Conversion Ratios

2 MHz operation optimized for automotive infotainment system design requirements

PHOENIX, Ariz. – Apr. 23, 2012 – ON Semiconductor (Nasdaq: ONNN), a premier supplier of high performance silicon solutions for energy efficient electronics, has introduced a new series of switching buck regulators for space-constrained, electromagnetic compatibility (EMC) sensitive automotive entertainment and infotainment applications. These highly integrated devices offer industry leading conversion ratios for battery connected switch-mode power supplies.

Download: JPG - 629.3kB  

Related Product:  NCV890201 


NCV4770x Adjustable Output Low Dropout Voltage Regulator ICs
ON Semiconductor Introduces New Series of Adjustable Output Low Dropout Voltage Regulators for Automotive Applications

Highly integrated devices deliver a more compact, cost effective solution for power management in automotive subsystems

PHOENIX, Ariz. – Feb. 22, 2012 – ON Semiconductor (Nasdaq: ONNN), a premier supplier of high performance silicon solutions for energy efficient electronics, has announced two new low dropout (LDO) voltage regulator ICs. Building on the company’s market-leading power management portfolio for automotive applications, the new devices are ideal for use in audio and infotainment systems, instrument cluster, navigation and satellite radio.

Download: JPG - 663.7kB  

Related Products:  NCV47700  NCV47701 


NCV8871 non-synchronous boost controller
Wide Input Automotive Non-Synchronous Boost Controller

PHOENIX, Ariz. – August 22, 2011 – ON Semiconductor (Nasdaq: ONNN), a premier supplier of high performance silicon solutions for energy efficient electronics, today introduced a new adjustable output non-synchronous boost controller for automotive systems.

Download: JPG - 482.1kB  

Related Product:  NCV8871 


New very low and ultra low-dropout (LDO) linear voltage regulators
ON Semiconductor Expands its Automotive LDO Voltage Regulator Portfolio with Five New Integrated Devices

PHOENIX, Ariz. – July 20, 2011 – ON Semiconductor (Nasdaq: ONNN), a premier supplier of high performance silicon solutions for energy efficient electronics, has announced the launch of five new very low and ultra low-dropout (LDO) linear voltage regulators to address a wide range of automotive applications such as rear camera modules, instrument clusters, and body and chassis applications.  These new devices deliver 150 milliamperes (mA) of output current, in space saving integrated solutions that meet the latest requirements from car manufacturers for very low quiescent currents when the ignition is switched off.

Download: JPG - 551.3kB  

Related Products:  NCV8667  NCV8668  NCV8669 


low dropout (LDO) linear voltage regulators
ON Semiconductor Expands its Portfolio of Voltage Regulators

PHOENIX, Ariz. – June 8, 2011 – ON Semiconductor (Nasdaq: ONNN) a premier supplier of high performance silicon solutions for energy efficient electronics has announced the introduction of five ultra small package, low dropout (LDO) linear voltage regulators to bolster its existing portfolio for smart phones and other portable electronics. Based on complementary metal oxide semiconductor (CMOS) technology, the new devices can each deliver an output current of 150 milliamperes (mA).

Download: JPG - 668.5kB  

Related Product:  NCP4681 


Low Dropout (LDO) Linear voltage Regulator
ON Semiconductor Introduces Wide Range of New LDO Linear Voltage Regulators Including Ultra-Small XDFN Packaged Devices

PHOENIX, Ariz. – Mar. 16, 2011 – ON Semiconductor (Nasdaq: ONNN) a premier supplier of high performance silicon solutions for energy efficient electronics has introduced three new families of wide input voltage, low dropout (LDO) Linear Voltage Regulators. The company’s strong capability in this area has been further strengthened by the addition of new devices to its popular NCP58x portfolio.

Download: JPG - 280.3kB  

Related Product:  NCP4586 


Image of the new AMIS-30523 which integrates a stepper motor driver and CAN transceiver in a single package, two-die device
ON Semiconductor Expands Innovative Solutions for Industrial Sector Applications with Launch of Two New Products at Electronica 2010

Company announces first-of-its-kind integrated stepper motor / CAN transceiver and new high power PoE-PD Interface Controller family

Electronica – MUNICH, Germany – Nov. 8, 2010 – ON Semiconductor (Nasdaq: ONNN), a premier supplier of high performance silicon solutions for energy efficient electronics, has announced the launch of two important new products specifically targeted at the industrial market sector at Electronica 2010. Designed for enabling current and future generation home and office automation applications, ON Semiconductor’s broad portfolio of industrial devices gives market-leading levels of ruggedness and reliability in addition to supporting the drive for low power, high efficiency design.

Download: JPG - 552.3kB  

Related Product:  AMIS-30523 


New family of high efficiency 2 ampere (A) to 4A integrated synchronous regulators
High Efficiency Synchronous Regulators in Compact Package

New regulators optimized specifically to meet the demands of high efficiency power system designs in consumer electronics

PHOENIX, Ariz. – June 23, 2010 – ON Semiconductor (Nasdaq: ONNN) a premier supplier of high performance, energy efficient silicon solutions, today introduced a new family of high efficiency 2 ampere (A) to 4A integrated synchronous regulators for consumer electronics applications such as set top boxes, DVD/hard disk drives, LCD monitors/TVs, speakerphones, cable modems, and telecom/datacom equipment.

Download: JPG - 293.9kB  

Related Products:  NCP3125  NCP3127  NCP3126 


New Synchronous PWM Controllers for Consumer and Industrial Applications
ON Semiconductor Launches New Synchronous PWM Controllers for Consumer and Industrial Applications

New solutions provide flexibility, choice of functionality and specifications, and a wide selection of input voltage ranges – all helping simplify implementation

PHOENIX, Ariz. – April 22, 2010 – ON Semiconductor (Nasdaq: ONNN) a premier supplier of high performance, energy efficient silicon solutions for green electronics  today introduced three new flexible synchronous pulse width modulation (PWM) controller devices the NCP3020A, NCP3020B and NCP3011. Offering a wide input voltage range, from  4.7V to 28V, these devices enable the flexibility to be used with a variety of input sources in consumer electronic equipment such as set-top-boxes and LCD televisions, as well as industrial and computing applications including printers, scanners and telecom systems.

Download: JPG - 475.4kB  

Related Products:  NCP3011  NCP3020 


NCP508 - a low current voltage regulator
ON Semiconductor Introduces a New Integrated Voltage Regulator that Offers a Low-Power Solution for Battery Powered Applications

50 mA Low Drop Out Linear Voltage Regulator offers high ripple rejection, excellent noise performance and a fast turn on time.

PHOENIX, Ariz. – March 31, 2010 – ON Semiconductor (Nasdaq: ONNN), a premier supplier of high performance, energy efficient silicon solutions for green electronics, today introduced the NCP508 – a low current voltage regulator that offers an efficient and economical solution to generating a low power voltage rail. The new regulator provides a solution that supports low power, space efficient and cost-effective designs in applications such as touch screens, keypads, smart phones, portable meters, printers and remote controls.

Download: JPG - 560.3kB  

Related Product:  NCP508 


New CMOS linear voltage regulator families from ON Semiconductor
ON Semiconductor New CMOS linear voltage regulator families

New CMOS voltage regulators enable next generation of portable battery-powered and ‘always on’ products

PHOENIX, Ariz. – March 23, 2010 – ON Semiconductor (Nasdaq: ONNN) a premier supplier of high performance, energy efficient silicon solutions for green electronics has extended its product portfolio, with the introduction of five new CMOS linear voltage regulator families. The NCP69x families are optimized for use in low current consumption portable battery-powered and ‘always on’ applications such as cable modems, satellite receivers, digital-set-top boxes and electricity meters.

Download: JPG - 531.1kB  

Related Product:  NCP693 



Your request has been submitted for approval.
Please allow 2-5 business days for a response.
You will receive an email when your request is approved.
Request for this document already exists and is waiting for approval.