Others




Intelligent Technologies Power Every Node in Next-gen Server

PHOENIX, – Sep.13, 2021 – Ramaxel, a leading supplier of server, storage and design service solutions, has selected intelligent cloud power technologies from onsemi (Nasdaq: ON) for its upcoming Intel-based VR13.HC servers. Power requirements are increasing in each successive processor generation. With their broad portfolio of high performance, high reliability cloud power solutions, onsemi is well positioned to deliver on such requirements.

Download: JPG - 558.3kB  JPG - 85.3kB  

Related Product:  FD3501MNTXG 


16 Mp Image Sensor for Factory Automation and ITS

PHOENIX, Ariz. – July 27, 2021 – ON Semiconductor (Nasdaq:ON) introduced the latest addition to the XGS series of CMOS image sensors. The XGS 16000 is a 16 Megapixel (Mp) sensor that provides high quality, global shutter imaging for factory automation applications including robotics and inspection systems. Consuming only 1 Watt at 65 frames per second (fps), the XGS 16000 delivers exceptional performance at low power. This makes the XGS 16000 one of the best in class for power consumption, while also offering one of the highest resolutions available for standard 29 x 29 mm industrial cameras.


QCS-AX-Chipset
Advanced Multi-Network 5G Router Powered by ON Semiconductor

ON Semiconductor (Nasdaq: ON) today announced that Sierra Wireless (NASDAQ: SWIR) (TSX: SW), a world-leading IoT solutions provider, has selected QCS-AX Wi-Fi 6 chipsets to power the Wi-Fi functionality of its market-leading XR Series of multi-network 5G routers.

Download: JPG - 289.6kB  


LED Drivers Add Intelligence to Connected Lighting

PHOENIX, Ariz. – June 21, 2021 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, has announced two new devices designed to enhance the performance of connected lighting systems. The NCL31000 and NCL31001 LED drivers allow manufacturers to develop LED luminaires with light-based positioning technology and visible light communication. By adding data intelligence and accurate positioning (up to 30 cm), these solutions will revolutionize lighting in a variety of spaces including supermarkets, warehouses, hospitals, and airports.

Related Products:  NCL31000  NCL31001 


XGS CMOS Image Sensors for High-Resolution Industrial Imagin

PHOENIX, Ariz. – 19 October, 2020 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, has expanded their XGS family of image sensors with high performance, low noise products that offer 12-bit image quality at a high frame rate. The new offerings include the XGS 45000 , the XGS 30000 and the XGS 20000 , which provide detailed imaging with up to 45 Mp for resolution critical applications and up to 60 fps in 8K video mode. Also available is the new XGS 5000 , designed with low power performance and state-of-the art image quality for compact 29 x 29 mm2 camera designs. Alongside the XGS 5000, 3 Mp and 2 Mp variants have been released for production.


CMOS Global Shutter Image Sensor for Machine Vision and M/R

PHOENIX, Ariz. – 7 October, 2020 – ON Semiconductor (Nasdaq:ON), driving energy efficient innovations, has introduced the AR0234CS 2.3 Mp CMOS image sensor with global shutter technology. The high-performance sensor is designed for a variety of applications including machine vision cameras, AR/VR/MR headsets, autonomous mobile robots (AMRs) and barcode readers.

Download: JPG - 79.9kB  



In-Cabin Monitoring System with Ambarella/Eyeris at AutoSens

AutoSens – Brussels, BELGIUM - 17 September, 2019 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, will feature a complete in-cabin monitoring system inclusive of driver monitoring and occupancy monitoring functions at AutoSens Conference in Brussels, Belgium. The demonstration includes multiple sensor types from ON Semiconductor - the 1 Megapixel (MP) Global Shutter AR0144AT image sensor and three 2.3 MP RGB-IR image sensors.

Related Product:  AR0144AT 


ON Semiconductor announces the introduction of the ARX3A0

The ARX3A0 digital image sensor with 0.3 Mega-Pixel (MP) resolution in a 1:1 aspect ratio. With up to 360 frames per second (fps) capture rate it can perform like a global shutter in many conditions but with the size, performance and responsivity benefits of being a Back-Side Illuminated (BSI) rolling shutter sensor. With its small size, square format and high frame rate, ARX3A0 is particularly suitable for emerging Machine Vision, Artificial Intelligence and AR/VR applications, as well as small supplemental security cameras.

Download: JPG - 369.7kB  

Related Product:  ARX3A0 


‘Innovations in Smart Homes and Buildings’

PHOENIX, Ariz. – July 17, 2019 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, is pleased to announce a new series of Technical Seminars for engineers and product designers of all skill levels. The seminars will be hosted in key locations worldwide and feature leading experts sharing their knowledge through technically rich and practical presentations and hands-on demonstrations.

Download: JPG - 217.0kB  


Battery-less IoT a Reality with RSL10 Multi-Sensor Platform

ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, continues to enable battery-less and maintenance-free IoT with the introduction of its RSL10 Multi-Sensor Platform powered solely with a solar cell. This complete solution supports the development of IoT sensors using continuous solar energy harvesting to gather and communicate data through Bluetooth® Low Energy, without the need for batteries or other forms of non-renewable energy.

Download: JPG - 390.8kB  


New Industrial and Automotive Qualified SiC MOSFETs

APEC 2019 – Booth 611 - ANAHEIM, USA – 13 March, 2019 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, has introduced two new silicon carbide (SiC) MOSFET devices. The industrial grade NTHL080N120SC1 and AEC-Q101 automotive grade NVHL080N120SC1 bring the enabling, wide-ranging performance benefits of wide band gap technology to important high growth end application areas such as Automotive DCDC and onboard charger applications for electric vehicles as well as solar, and uninterruptible and server power supplies.

Download: JPG - 329.3kB  

Related Products:  NTHL080N120SC1  NVHL080N120SC1 


ON Semiconductor Introduces the RSL10 Sensor Development Kit

NUREMBERG, Germany – 13 February, 2019 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, is pleased to announce the introduction of the RSL10 Sensor Development Kit, designed to provide engineering teams with a comprehensive platform for developing IoT applications with cutting-edge smart sensor technology, and enabled by the industry’s lowest power Bluetooth Low Energy radio.


ON Semiconductor Announces Strata Developer Studio™

CES 2019 – Las Vegas, NV – 02 January, 2019 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, is announcing the introduction of the Strata Developer Studio™, a first-of-its-kind cloud-based development platform that provides a seamless, personalized and secure environment for engineers to evaluate and design with ON Semiconductor technologies.

Download: JPG - 389.6kB  


New Energy Harvesting Bluetooth® Low Energy Switch

Download: JPG - 315.6kB  JPG - 56.0kB  


New Development Support for RSL10 Bluetooth 5 Radio Family

ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, has extended the capabilities of its RSL10 family of Bluetooth 5 certified radio System-on-Chips (SoCs) with support for the Bluetooth SIG mesh networking standard. In addition, the company has introduced a new PC software application with the RSL10 USB dongle. Alongside the recently-announced RSL10 SIP, the additional software and design support tools ease development and enable support for a broad range of industrial and consumer applications.

Download: JPG - 404.3kB  


50 MP CCD Image Sensor for Inspection of Smartphone Displays

PHOENIX, Ariz. – October 29, 2018 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, is enabling more efficient inspection of smartphone displays with the introduction of a new 50 megapixel (MP) resolution charge-coupled device (CCD) image sensor. As the highest resolution Interline Transfer CCD image sensor commercially available, the KAI-50140 provides the critical imaging detail and high image uniformity needed not only for inspection of smartphone displays but also circuit board and mechanical assembly inspection as well as aerial surveillance.

Download: JPG - 228.0kB  

Related Product:  KAI-50140 


Bluetooth® 5 Radio Family Expands with SiP Module

Phoenix, Arizona – September 11, 2018 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, has extended its RSL10 family of Bluetooth 5 certified radio System-on-Chips (SoCs) with a ready-to-use 6 x 8 x1.46 mm System-in-Package (SiP) module . Supporting Bluetooth low energy wireless profiles, RSL10 devices can be easily designed into any ‘connected’ application including sports / fitness or mHealth wearables, smart locks and appliances.

Download: JPG - 447.5kB  JPG - 58.9kB  

Related Product:  RSL10 SIP 


SiC Diodes for Demanding Automotive Applications

PCIM 2018 – Hall 9 Booth #342 – Nuremberg, Germany – 5 June, 2018 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, has announced an expansion of its silicon carbide (SiC) Schottky diode portfolio to include devices specifically intended for demanding automotive applications. The new AEC-Q101 automotive grade SiC diodes deliver the reliability and ruggedness needed by modern automotive applications, along with the numerous performance benefits synonymous with Wide Band Gap (WBG) technologies.

Download: JPG - 1177.9MB  



New Battery-Free Smart Passive Sensors™ Development Kit

Consumer Electronics Show (CES) - Venetian 3302 – Las Vegas, NV – Jan. 8, 2018 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, has announced a complete wireless battery free sensing solution kit (SPSDEVK1) that allows the company’s innovative Smart Passive Sensors™(SPS) to be rapidly integrated into Internet-of-Things (IoT) applications.

Download: JPG - 265.2kB  


ON Semiconductor Introduces Preconfigured Development Suite

EUHA 2017 – Hall 4A, Booth D02 – Nuremberg, Germany – October 17, 2017 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, continues to grow its broad portfolio of ultra-low-power solutions for the hearing health industry by unveiling the Ezairo Preconfigured Suite (Pre Suite), a development toolkit enabling turnkey solutions based on the company’s Ezairo 7100 Digital Signal Processor (DSP).

Download: JPG - 303.5kB  

Related Product:  EZAIRO 7150 SL 


Sigfox Verified RF System-in-Package for Low Power IoT

Sigfox World IoT Expo – Booth #4 - Prague, Czech Republic – September 25, 2017 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, has announced a new programmable RF transceiver System in Package (SiP) integrating an advanced RF System-on-Chip (SoC) with all surrounding Bill of Material (including a TCXO). The AX-SIP-SFEU provides the most integrated Sigfox solution for both uplink (transmit) and downlink (receive) communications. The device is the first in a new family of SiPs that will be launched over the coming months, providing a comprehensive range of ready-to-use, turnkey radio frequency (RF) solutions to support applications requiring Internet of Things (IoT) connectivity.

Related Product:  AX-SIP-SFEU 


Sampling Industry’s Lowest Power Bluetooth® Low Energy SoC

Mobile World Congress - BARCELONA, Spain – February 23, 2017 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, has positioned itself at the forefront of ultra-low-power wireless connectivity with its latest product offering. The RSL10 highly flexible, ultra-miniature multi-protocol Bluetooth 5 certified radio System-on-Chip (SoC) is capable of supporting the advanced wireless functionalities emerging in the IoT and Connected Health & Wellness sectors without compromising battery life or overall system size. Target applications for this device include wearables such as fitness trackers and smart watches, smart locks, and electronics like lighting or appliances.

Download: JPG - 293.8kB  

Related Product:  RSL10 


Highly Integrated Capacitive-Digital Converter

PHOENIX, Ariz. – Jan.17, 2017 - ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, has introduced a new touch/proximity sensing solution that combines industry-leading performance, cost-effectiveness and convenience in a single chip. The LC717A30UJ high dynamic range capacitance-to-digital converter uses mutual capacitance to detect changes in capacitance down to femtofarad (fF) levels. Parasitic capacitance cancellation raises the detector sensitivity, while its built-in noise rejection mechanism combats the effects of electro-magnetic interference (EMI).

 

Download: JPG - 75.8kB  JPG - 593.5kB  

Related Product:  LC717A30UJ 


Design Platform for Next Generation Wearable Technology

PHOENIX, Ariz. – Nov. 29, 2016 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, has utilized its strength and depth in a broad range of semiconductor disciplines - including analog, power management, sensor interface and signal conditioning - to introduce a comprehensive development resource for the wearable electronics sector. The new Download: PNG - 2234.2MB  


Most Compact Intelligent Power Module for Automotive

Electronica - MUNICH, Germany – Nov. 7, 2016 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, and a top 10 global automotive semiconductor supplier following its recent acquisition of Fairchild Semiconductor, has introduced the industry’s most compact 650 volt (V), 50 ampere (A) automotive qualified intelligent power module for controlling vehicle air conditioning (A/C) compressors. The FAM65V05DF1 addresses numerous other high voltage auxiliary motor applications in hybrid and electric vehicles and helps designers increase the performance and efficiency of applications while simultaneously reducing costs.

Download: JPG - 156.8kB  


Modular Development Platform for Internet of Things

Electronica - MUNICH, Germany – Nov. 7, 2016 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, has introduced a modular IoT Development Kit (IDK) that provides engineers with all of the hardware and software building blocks needed to speed the evaluation, design and implementation of medical, home, and industrial IoT applications.

Download: JPG - 690.9kB  


Advanced, Integrated Solutions for Power Management

Electronica - MUNICH, Germany – Nov. 7, 2016 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, has launched new intelligent power module (IPM) technologies for industrial power management and motor control applications.

Download: JPG - 721.3kB  


Low-cost, compact image sensors for Industrial applications

PHOENIX, AZ – Nov. 1, 2016 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, is bringing the advanced global shutter imaging performance of the PYTHON CMOS image sensor family to a cost-effective, small-footprint design.

Download: JPG - 282.1kB  

Related Product:  PYTHON480 


New Options for Low-Light Industrial Imaging Applications

PHOENIX, AZ – Sept. 27, 2016 – ON Semiconductor (Nasdaq: ON ), driving energy efficient innovations, has announced three new devices for driving3-phase BLDC motors via 180 degree sinusoidal waveforms. Designed for use in cooling fans of household appliances such as refrigerators, as well as games consoles and computing equipment, the LV8811, LV8813, and LV8814 have voltage ranges of 3.6 volts (V) to 16 V, 6 to 16 V, and 3.6 to 16 V respectively. These highly integrated, software-lessmotor driverssimplify motor control circuit design by eliminating software development time. In addition, these devices reduce acoustic noise and vibration, and enable deployment of energy efficient motor controls. They can be controlled by a single Hall sensor, reducing system costs. Motor speed can be set by either a pulse width modulated (PWM) signal or a DC voltage. Furthermore, their lead angle can easily be adjusted.

Download: JPG - 994.0kB  

Related Products:  KAE-02150  KAE-08151 


Ultra Field Stop trench technology
New Scope of IGBT Offering with 1200 V Devices

PCIM - Nuremberg, Germany. – May 10, 2016 ON Semiconductor Corporation (Nasdaq: ON), driving energy efficiency innovations, has introduced a new series of insulated gate bipolar transistors (IGBTs) which utilize its proprietary Ultra Field Stop trench technology. The NGTB40N120FL3WG, NGTB25N120FL3WG and NGTB40N120L3WG are designed to deliver elevated levels of operational performance in order to meet the exacting demands of modern switching applications. These 1200 volt (V) devices are able to achieve industry-leading total switching loss (Ets) characteristics; the remarkable improvement in performance is attributable in part to a very wide highly activated field-stop layer & optimized co-pack diode.

Download: JPG - 541.5kB  


Multifaceted IoT Sensor Platform for Battery-Free Operation
Multifaceted IoT Sensor Platform for Battery-Free Operation

Mobile World Congress (MWC) – Barcelona, Spain – Feb. 22, 2016 – ON Semiconductor (Nasdaq: ON ),driving energy efficiency innovations, teamed with RFMicron, and developed a game-changing ‘plug-and-play’ development tool to speed the deployment of wireless passive sensor solutions onto any Internet of Things (IoT) cloud platform. The IoT Platform Development Kit, SENSORRFGEVK, brings together a series of performance-optimized computing and connectivity modules to facilitate quick and effective deployment of battery-free wireless sensing technology and IoT hardware in locations where power and space constraints are of particular concern. This streamlined and flexible solution takes the approach of moving much of the system’s intelligence away from where the sensors are situated, and placing it on the cloud.

Download: PNG - 965.4kB  PNG - 95.1kB  


Advanced Audio-Processor from ON Semiconductor
Advanced Audio-Processing SoC Delivers Superior Performance

PHOENIX, Ariz. – October 27, 2015 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, has released its latest high-resolution audio processing System-on-Chip with 1656KB SRAM and power-efficient hardware acceleration, bringing extra space savings and longer battery life to devices such as smartphones, wearable accessories and voice recorders.

Download: JPG - 619.1kB  

Related Product:  LC823450 


ON Semiconductor Unveils 1080p Video Development Kit for IoT

PHOENIX, Ariz. – October 13, 2015 – ON Semiconductor (Nasdaq: ON ), driving energy efficient innovations, has introduced an open imaging platform for low power video streaming applications. The MatrixCam™ video development kit (VDK) has been developed specifically to encourage greater video adoption within Internet of Things (IoT) products, as well as accelerating OEMs’ time to market. Among its key applications are home automation systems, building access devices, baby monitors, advanced lighting controls and smart appliances. MatrixCam video development kit hardware and software design documents are available for download from ON Semiconductor and its partners’ portal.

Download: JPG - 17.7kB  

Related Product:  AR023Z 


High Performance, High Density Power Integrated Modules
High Performance, High Density Power Integrated Modules

PCIM - Nuremberg, Germany. – May 19, 2015 – ON Semiconductor (Nasdaq: ONNN), driving energy efficiency innovations, has introduced a state-of-the-art 80 ampere (A) Power Integrated Module (PIM) with industry leading performance for demanding uninterruptable power supplies (UPS), industrial variable frequency drives, and solar inverter applications.

Download: JPG - 707.7kB  


New Medium Voltage N-Channel MOSFETs
Comprehensive Array of New Medium Voltage N-Channel MOSFETs

PCIM - Nuremberg, Germany. – May 19, 2015 – ON Semiconductor (Nasdaq: ONNN), ON Semiconductor (Nasdaq: ON), driving energy efficiency innovations, has further expanded its broad portfolio of power MOSFETs with new, high efficiency single n-channel devices targeted at data networking, telecommunications and industrial applications.

Download: JPG - 66.3kB  JPG - 533.8kB  


ON Semiconductor's Family of Ultra-Low Power Precision Operational Amplifiers
ON Semiconductor Unveils New Family of Ultra-Low Power Precision Operational Amplifiers

New zero drift, low voltage devices highly suited to precision applications in industrial, consumer, wireless, IoT and automotive where strong stability across wide operating temperature ranges is mandated

Download: JPG - 838.7kB  

Related Products:  NCS325  ncs333 


Ultra-low power wireless transceiver
Low Power, Integrated Wireless Device for Connectivity, IoT

European Utility Week – AMSTERDAM, Netherlands – Nov. 3, 2014 – ON Semiconductor (Nasdaq: ONNN), driving energy efficiency innovations, is using this year’s European Utility Week Exhibition and Conference as the forum to launch an important new product family that supports high-performance, reliable and efficient communications for the Internet of Things (IoT) and smart metering applications. The NCS3651x family of system-on-chip (SoC) transceivers has been developed using ON Semiconductor’s expertise in highly integrated mixed signal integrated device technology and radio frequency (RF) design. The company is also an active member of the ZigBee® Alliance.

New standards compliant NCS3651x family of system-on-chip (SoC) transceivers support communications for the IoT and smart metering

Download: JPG - 693.5kB  

Related Product:  NCS36510 


Struix High Performance SiP Solution for Portable Medical Devices
High Performance SiP Solution for Portable Medical Devices

Semi-customizable, power efficient SiP solution enables miniature sensing systems ideal for mHealth applications including glucose monitors, heart rate monitors, and electrocardiogram analyzers

PHOENIX, Ariz. – Sept. 15, 2014 – ON Semiconductor (Nasdaq: ONNN), driving energy efficiency innovations, has responded to rapidly-evolving product development demands within the portable medical market by introducing Struix, a semi-customizable System-in-Package (SiP) solution for precision sensing and monitoring in a variety of mobile medical electronics including glucose monitors, heart rate monitors and electrocardiogram analyzers.

Download: JPEG - 1282.0MB  


KAI-08051 CCD Image Sensor
CCD Image Sensor for ITS, Surveillance, Industrial Inspection

PHOENIX, AZ. - July 14, 2014 – ON Semiconductor (Nasdaq: ONNN), driving energy efficient innovations, is enhancing the charge-coupled device (CCD) image sensor portfolio recently acquired from Truesense Imaging with new technology that improves imaging performance for industrial applications.

Download: JPG - 621.6kB  

Related Product:  KAI-08051 


Highly Integrated, Low Power HART CMOS Modem IC
Highly Integrated, Low Power HART CMOS Modem IC

PHOENIX, Ariz. – June 9, 2014 – ON Semiconductor (Nasdaq: ONNN), driving energy efficiency innovations, has expanded its family of modems targeted at highway addressable remote transducer (HART) industrial communication implementations. With this latest product introduction, ON Semiconductor, who recently became a member of the HART foundation (www.hartcomm.org), now offers solutions for low power HART applications.

Download: JPG - 737.5kB  

Related Product:  NCN5193 


Power MOSFET image
New Family of Low Voltage Power MOSFETs

Power Conversion Intelligent Motion (PCIM) – NUREMBERG, Germany – May 20, 2014 – ON Semiconductor (Nasdaq: ONNN), driving energy efficient innovations, has introduced a new family of six N-channel Metal Oxide Semiconductor Field Effect Transistors (MOSFETs) that have been designed and optimized to deliver industry leading efficiency compared to existing devices on the market.

Download: JPG - 294.8kB  

Related Products:  NTMFS4H01N  NTMFS4H01NF 


ESD Protection Array Photo
Low Capacitance, Low Clamping Voltage ESD Protection Devices

PHOENIX, Ariz. – April 16, 2014 – ON Semiconductor (Nasdaq: ONNN), driving innovation in energy efficiency, has introduced five new electrostatic discharge (ESD) suppression devices for today’s most advanced interfaces. Patent-pending design techniques and process technology enable these devices to deliver the industry’s lowest capacitance and ESD clamping voltage, suitable for use with extremely high data rate interfaces and small geometry chipsets.

Download: JPG - 319.2kB  

Related Product:  ESD8004 


Preconfigured DSP System for Hearing Health
Expanded RHYTHM Portfolio of DSPs for Hearing Aid Market

AudiologyNOW! – Orlando, Florida - March 25, 2014 – ON Semiconductor (Nasdaq: ONNN), driving energy efficient innovations, has added two new devices to its RHYTHM™ family of preconfigured Digital Signal Processing (DSP) systems designed specifically for use in hearing aid devices.

Download: JPG - 288.2kB  

Related Product:  Rhythm R3920 


integrated slave transceiver photo
Integrated Slave Transceiver for M-BUS Remote Metering Applications

Efficient and rugged NCN5150 transceiver is ideal for remote meter reading applications including multi-energy, heating and cooling, water meters and gas meters

PHOENIX, Ariz. – September 9, 2013 – ON Semiconductor (Nasdaq: ONNN), driving innovation in energy efficiency, has introduced a new integrated slave transceiver for use in two-wire Meter Bus (M-BUS) slave devices and repeaters. The NCN5150 provides all necessary functionality to satisfy the EN 13757-2 and EN 1434-3 standards that describe the physical layer requirements for remote meter reading M-BUS applications in multi-energy, heating and cooling, water and gas meters.

Download: JPG - 457.5kB  

Related Product:  NCN5150 


Integrated Record and Playback Device for Portable Applications
Integrated Record/Playback Device for Portable Applications

LC823430TA audio processing system incorporates DSP, audio CODEC, plus numerous other analog blocks and is supported by application software to help speed customer product development

PHOENIX, Ariz. – June 4, 2013 – – ON Semiconductor (Nasdaq: ONNN), driving innovation in energy efficiency, has introduced a new MP3 capable device to support both record and playback in portable MP3 audio applications where there is a strong requirement for miniaturization, reduced bill of materials (BoM) and reduced cost. The LC823430TA audio processing system provides a single-chip solution by integrating digital signal processing (DSP) circuitry for MP3 encoding and decoding, and analog blocks such as audio analog-to-digital conversion (ADC) and digital-to-analog conversion (DAC).

Download: JPG - 265.1kB  

Related Product:  LC823430TA 


New LGA-Packaged MOSFETs Help Maximize Efficiency
New LGA-Packaged MOSFETs Help Maximize Efficiency

Single and dual Li-ion battery charging / discharging protection circuits benefit from high-performance FlipChip MOSFETs

PHOENIX, Ariz. – June 4, 2013 – – ON Semiconductor (Nasdaq: ONNN),driving innovation in energy efficiency,has introduced two new MOSFET devices designed for use in smart phone and tablet PC applications where they provide a crucial part of the Lithium ion (Li-ion) battery charging / discharging protection circuit switching. The EFC6601R and EFC6602R help designers to reduce solution size, improve efficiency and maximize battery life.

Download: JPG - 139.7kB  


New Field Stop II (FSII) devices improve switching characteristics and reduce losses by up to 30 percent.
Industry Leading Performance Expansion to IGBT Portfolio

Power Conversion Intelligent Motion (PCIM), NUREMBERG, Germany – May 14, 2013 – – ON Semiconductor (Nasdaq: ONNN),driving innovation in energy efficiency, continues to expand its portfolio of high performance IGBTs targeted at high performance power conversion (HPPC) consumer appliance and industrial applications. The new generation Field Stop II (FSII) devices being launched at PCIM improve switching characteristics and reduce losses by up to 30 percent leading to higher efficiency and translating into lower case temperature, giving designers options for improving overall system performance and reliability. Optimized for targeted applications, these devices show a reduction in case temperature of up to 20 percent over existing devices.

Download: JPG - 317.0kB  

Related Products:  NGTB20N120IHR  NGTB20N135IHR 


Image of Tunable RF Components (TRFC)
Tunable RF Components for Smartphones

Tunable RF Components allow smaller volume antennas, reduced power consumption and support increasing mobile data demands in the latest generation of smartphones

PHOENIX, Ariz. - March 5, 2013 – ON Semiconductor (Nasdaq: ONNN), driving energy efficient innovations, has introduced a new family of Tunable RF Components (TRFC) that address the design challenges faced by engineers developing the latest generation smartphones. The new devices optimally combine tuning range, RF quality factor (Q) and frequency operation, providing a superior solution to existing fixed approaches.

Download: JPG - 548.1kB  

Related Products:  TCP-3012H  TCC-103 


Video Signal Processor ICs for Small LCD Panels
Video Signal Processor ICs for Small LCD Panels

PHOENIX, Ariz. – Jan. 10, 2013 – ON Semiconductor (Nasdaq: ONNN), driving innovation in energy efficiency, has released two new highly integrated image signal processor ICs ideal for use in applications such as vehicle reversing cameras, in-vehicle navigation systems and various consumer video monitoring security systems where small LCD screens are utilized. The LC749000PT for automotive applications and the LC749000AT for consumer products, support important end application energy savings and utilize advanced signal technology to improve the picture quality of digitally compressed images.

Download: JPG - 215.9kB  

Related Product:  LC749000AT 


High-Efficiency Stepper Motor Driver for Office Automation
High-Efficiency Stepper Motor Driver for Office Automation

PHOENIX, Ariz. – Dec. 19, 2012 – ON Semiconductor Nasdaq: ONNN),driving innovation in energy efficiency, has introduced the LV8702V, a new stepper motor driver IC that delivers significantly improved efficiency versus existing products on the market. The device has been specifically designed for office automation equipment applications such as copiers, scanners and multi-function printers.

Download: JPG - 66.0kB  

Related Product:  LV8702V 


1200 V Trench Field Stop IGBTs
High Performance 1200 V Trench Field Stop IGBT Expanded Portfolio

PHOENIX, Ariz. – Oct. 22, 2012 – ON Semiconductor (Nasdaq: ONNN), a premier supplier of high performance silicon solutions for energy efficient electronics, has expanded its NGBTxx family of 1200 volt (V) trench field stop (FS) insulated gate bipolar transistor (IGBT) devices with nine new energy efficient solutions.

Download: JPG - 604.5kB  

Related Products:  NGTB25N120FL  NGTB15N120FL  NGTB40N120FL  NGTB30N120IHL  NGTB40N120IHL  NGTB30N120L  NGTB40N120L  NGTB30N120IHS 


Industry's Smallest MOSFETs in Highly Compact Packages for Portable Applications
Industry's Smallest MOSFETs in Highly Compact Packages

PHOENIX, Ariz. – Oct. 16, 2012 – ON Semiconductor (Nasdaq: ONNN), a premier supplier of high performance silicon solutions for energy efficient electronics, has expanded on the company’s extensive interface and power management portfolio with the introduction of a pair of ultra small, ultra thin, small signal MOSFETs optimized for space-constrained portable consumer electronics such as tablet computers, smart phones, GPS systems, digital media players and portable games consoles.

Download: JPG - 640.4kB  

Related Products:  NTNS3193NZ  NTNS3A91PZ 


NCV7381 Single Channel FlexRay Transceiver
ON Semiconductor Introduces High Speed Bus Transceiver for Reliable Automotive Networking

Innovative new device supports latest version of FlexRay™ standard

PHOENIX, Ariz. – July 31, 2012 – ON Semiconductor (Nasdaq: ONNN), a premier supplier of high performance silicon solutions for energy efficient electronics, has expanded its portfolio of automotive networking products with the introduction of a bus transceiver IC that is compliant with the most recent adaption to the FlexRay™ communications protocol. The NCV7381 is a highly robust, single-channel device capable of data transfer speeds up to 10 megabits per second (Mbits/s). Conforming fully with FlexRay™ Electrical Physical Layer Specification Rev. 3.0.1, the new device offers a differential transmit and receive capability between the wired FlexRay™ communication medium and the protocol controller/host.

Download: JPG - 603.4kB  

Related Product:  NCV7381 


Power Line Carrier (PLC) Modem SoC
PLC Modem SoC for Smart Metering & Building Automation

Flexible NCN49597 utilizes ARM Cortex processor and innovative features to enhance communication robustness and versatility for e-metering, home automation, solar energy and lighting control

PHOENIX, Ariz. – June 19, 2012 – ON Semiconductor (Nasdaq: ONNN) a premier supplier of high performance silicon solutions for energy efficient electronics has introduced a new power line carrier (PLC) modem system-on-chip (SoC) for use in applications such as e-metering, home automation, solar energy and lighting control. The first device in a new family of PLC modems, the NCN49597 combines a low power 32-bit ARM Cortex M0 processor with a high-precision analog front end. Based on a dual 4800-baud S-FSK (Spread Frequency Shift Keying) channel technology, it has been optimized for power efficiency and performance, while providing excellent robustness and reliability to enable operation in the harshest environments.

Download: JPG - 784.5kB  

Related Product:  NCN49597 


Switching ICs for high frequency signals such as PCI Express 3.0 and DisplayPort 1.2 I/O signals
Low Quiescent Current Switches for High-Speed Interfaces

New product offerings meet signal integrity demands set by PCI Express 3.0 & DisplayPort 1.2 for notebook and desktop computing, server and network storage equipment applications

PHOENIX, Ariz. – March 27, 2012ON Semiconductor Corporation (Nasdaq: ONNN), a premier supplier of high performance silicon solutions for energy efficient electronics has introduced two new multiple-channel differential switching ICs in single pole, double throw (SPDT) switch configurations for high frequency signals such as PCI Express 3.0 and DisplayPort 1.2 I/O signals. Target applications include notebook computers, desktop computers, servers and network storage equipment.

Download: JPG - 675.8kB  

Related Products:  NCN3612B  NCN3411 


NMLU1210 High Efficiency Wireless Charging ICs
ON Semiconductor's High Efficiency Wireless Charging ICs

Full bridge rectifier with low Rds(ON) MOSFET sets new performance levels for wireless charging of cell phones, media tablets, portable media players, digital still cameras and GPS units

PHOENIX, Ariz. – March 20, 2012 – ON Semiconductor Corporation (Nasdaq: ONNN) a premier supplier of high performance silicon solutions for energy efficient electronics, has released the NMLU1210, an innovative power MOSFET integrated circuit (IC) for wireless charging applications in portable products such as cell phones, media tablets, portable media players, digital still cameras and GPS units.

Download: JPG - 524.2kB  

Related Product:  NMLU1210 


ON Semiconductor introduces of a new family of 100 volt (V) trench-based low forward voltage Schottky rectifiers</a> (LVFR) for applications such as switching power supplies.
Trench-Based Schottky Rectifiers Deliver Improved Switching

PHOENIX, Ariz. – Dec. 13, 2011 – ON Semiconductor (Nasdaq: ONNN), a premier supplier of high performance silicon solutions for energy efficient electronics, has introduced of a new family of 100 volt (V) trench-based low forward voltage Schottky rectifiers (LVFR) for applications such as switching power supplies for notebook adapters or flat panel displays, reverse battery protection circuits, and high frequency DC-DC converters.

Download: JPG - 297.3kB  

Related Products:  NTST30100CTG  NTST20100CTG  NTST20U100CTG 


NCV7425 LIN+LDO Transceiver
Integrated LIN+LDO and Dual CAN Transceivers

Automotive-qualified integrated circuits save space and system cost in vehicle comfort and convenience, and industrial designs

PHOENIX, Ariz. – Nov. 28, 2011 – ON Semiconductor (Nasdaq: ONNN), a premier supplier of high performance silicon solutions for energy efficient electronics, has introduced two new integrated transceiver devices for use in local interconnect network (LIN) and control area network (CAN) designs in automotive and industrial applications. Both the NCV7425 LIN+LDO transceiver and NVC7441 dual CAN transceiver offer a robust, space saving and cost-effective solution for next-generation automotive ‘convenience’ applications as well as LIN and CAN based industrial designs.

Download: JPG - 353.2kB  

Related Product:  NCV7425 


Industry's first 3:1 high speed USB switch supporting the new Mobile High Definition Link (MHLTM) interface standard for High Definition (HD) video and digital audio.
New High Speed 3:1 USB Mobile High Definition Link Switch

PHOENIX, Ariz. – Aug. 16, 2011 ON Semiconductor Corporation (Nasdaq: ONNN) a premier supplier of high performance silicon solutions for energy efficient electronics, has introduced the NCN1188, the industry’s first 3:1 high speed USB switch with the capacity to support the new Mobile High Definition Link (MHLTM) interface standard for High Definition (HD) video and digital audio.

Download: JPG - 334.3kB  

Related Product:  NCN1188 


New Class D Audio Amplifier Image
New Class D Audio Amplifier for LCD TVs

PHOENIX, Ariz. – Aug. 2, 2011 – ON Semiconductor (Nasdaq: ONNN) a premier supplier of high performance, silicon solutions for energy efficient electronics today introduced the NCS8353 stereo audio amplifier, a Class D device with high efficiency levels (>87%), that elimates the need for the inclusion of a heatsink in the system design. 

Download: JPG - 557.6kB  

Related Product:  NCS8353 


Serial EEPROM Memory CAT24M01 image
ON Semiconductor Expands Serial EEPROM Portfolio

PHOENIX, Ariz. – June 22, 2011 – ON Semiconductor (Nasdaq: ONNN) a premier supplier of high performance silicon solutions for energy efficient electronics, has released new EEPROM (Electrically Erasable Programmable Read-Only Memory) devices for the automotive, medical, and consumer markets.

Download: JPG - 429.1kB  

Related Product:  CAT24M01 


Common Mode Filter Image
Innovative Protected Common Mode Filters for High Speed Serial Interfaces

PHOENIX, Ariz. – May 24, 2011 – ON Semiconductor (Nasdaq: ONNN) a premier supplier of high performance silicon solutions for energy efficient electronics has introduced a new range of common mode filter (CMF) devices with integrated electrostatic discharge (ESD) protection to suppress noise and provide strong signal integrity. The new EMI2121, EMI4182 and EMI4183 devices are highly suitable for implementation in smartphones, media tablets, wireless connectivity dongles and digital camcorders, as well as set top boxes and DVD players.

Download: JPG - 697.1kB  

Related Products:  EMI4183  EMI4182  EMI2121 


New ESD Protection Diode image
ON Semiconductor Introduces Industry’s Lowest Capacitance ESD Protection for High Bandwidth Interfaces

PHOENIX, Ariz. – May 11, 2011 – ON Semiconductor (Nasdaq: ONNN) a premier supplier of high performance silicon solutions for energy efficient electronics, has released its newest product for integrated electrostatic discharge (ESD) protection for use in notebooks, tablets, and external storage devices.

Download: JPG - 642.6kB  

Related Product:  ESD7004 


Precision Mixed-Signal Microcontroller Image
ON Semiconductor Introduces Q32M210 Precision Mixed-Signal Microcontroller for Portable Sensing Applications

PHOENIX, Ariz. – May 2, 2011 – ON Semiconductor (Nasdaq: ONNN) a premier supplier of high performance silicon solutions for energy efficient electronics, has introduced the Q32M210, the first in a new family of mixed-signal microcontrollers for precision measurement and monitoring. Designed for use in portable sensing applications and built with the ARM® Cortex™-M3 processor, the highly-integrated Q32M210 provides a unique combination of high precision performance and predictable operation with exceptional power efficiency.

Download: JPG - 281.5kB  


Single Channel, Power MOSFETs
ON Semiconductor’s New Power MOSFET Devices Deliver Valuable Space Savings and Robust Performance for Automotive Modules

PHOENIX, Ariz. – Feb. 07, 2011 – ON Semiconductor (Nasdaq: ONNN) a premier supplier of high performance silicon solutions for energy efficient electronics today announced the introduction of six new AEC-Q101 qualified logic level, single channel, power MOSFETs for automotive module in small, flat lead packages.

Download: JPG - 559.4kB  

Related Products:  NVTFS4823N  NVTFS5116PL  NVTFS5811NL  NVTFS5826NL  NVTFS5820NL 


High Performance Voice Capture SoC
ON Semiconductor Unveils BelaSigna R261 High Performance Voice Capture System-on-Chip

PHOENIX, Ariz. – December 14, 2010 – ON Semiconductor (Nasdaq: ONNN) a premier supplier of high performance silicon solutions for energy efficient electronics today introduced BelaSigna R261. This complete system-on-chip (SoC) solution for portable consumer electronics incorporates a highly optimized digital signal processor (DSP) with an advanced dual-microphone noise reduction algorithm to improve speech intelligibility in noisy environments, while preserving voice naturalness.

Download: JPG - 377.6kB  

Related Product:  BELASIGNA R261 


The new NCV7321 is a fully featured local interconnect network (LIN) transceiver
ON Semiconductor Introduces Automotive Solutions for Next Generation Body Electronics Applications

Company introduces three new automotive devices at Electronica 2010 to address in-vehicle networking, LED Lighting, and load management

Electronica – MUNICH, Germany – Nov. 8, 2010 – ON Semiconductor (Nasdaq: ONNN), a premier supplier of high performance silicon solutions for energy efficient electronics, has announced the launch of three new products specifically targeted at the automotive market sector at Electronica 2010. All three devices support current and next generation body electronics applications.

Download: JPG - 471.9kB  

Related Product:  NCV7321 


NCP2704 audio subsystem IC
New Components from ON Semiconductor Support Development of High Efficiency Next Generation Portable and Consumer Electronics

Company introduces integrated Class D audio amplifiers and current limiting switch products for a wide range of portable and consumer applications.

Electronica MUNICH, Germany – Nov. 8, 2010 – ON Semiconductor (Nasdaq: ONNN), a premier supplier of high performance silicon solutions for energy efficient electronics, has announced four new products designed to support portable and consumer electronics applications.

Download: JPG - 585.5kB  

Related Product:  NCP2704 


NCS5650 - a new line driver device targeted at Power Line Carrier (PLC) communications applications
ON Semiconductor Introduces Compact Power Line Communication Solution for Reduced Component Count and Implementation Cost

Complies with global regulatory standards including CENELEC

PHOENIX, Ariz. – Aug. 11, 2010 – ON Semiconductor (Nasdaq: ONNN) a premier supplier of high performance, energy efficient silicon solutions, introduced the NCS5650 -  a new line driver device targeted at Power Line Carrier (PLC) communications applications such as smart metering, industrial control and street lighting. The NCS5650 is a high efficiency, Class AB, low distortion driver, specifically designed to drive power line mains and capable of accepting a signal from any power line carrier modem.

Download: JPG - 576.0kB  

Related Product:  NCS5650 


N-channel power MOSFET image
ON Semiconductor Extends High-Voltage Power Solutions Offerings with 30 Volt N-Channel Power MOSFETs with Integrated Schottky Diodes

Innovative monolithic design brings improved system efficiency and reduces EMI noise

PHOENIX, Ariz. – April 6, 2010 – ON Semiconductor (Nasdaq: ONNN) a premier supplier of high performance, energy efficient silicon solutions for green electronics, today broadened its portfolio of N-channel power MOSFET devices with the introduction of new 30 V products with integrated Schottky diodes.

Download: JPG - 969.5kB  

Related Product:  NTMFS4897N 


ON Semiconductor Expands High-Voltage MOSFET Portfolio
ON Semiconductor Expands High-Voltage MOSFET Portfolio

Robust 500 volt and 600 volt MOSFETs deliver fast turn-on and reduce dynamic power losses for high-voltage power consumer and industrial applications

PHOENIX, Ariz. – Feb. 11, 2010 – ON Semiconductor (Nasdaq: ONNN) a premier supplier of high performance, energy efficient silicon solutions for green electronics today has expanded its market leading power switching product offering with the introduction of a high-voltage power MOSFET portfolio including 500 volt (V) and 600 V devices. These new solutions are designed for the robust needs of high voltage, energy conversion applications such as Power Factor Correction (PFC) and Pulse Width Modulation (PWM) stages, where faster turn-on and reduced dynamic power losses are crucial. Specifically, they are ideal for use in power adapters for gaming, printing and notebooks, as well as implementation in ATX power supplies, LCD panel power and industrial lighting ballast.

Download: JPG - 534.2kB  

Related Product:  NDF10N60Z 


N-channel power MOSFET photo Web version
ON Semiconductor Expands 100 V MOSFET Portfolio

100 percent avalanche tested MOSFETs deliver industry-leading ratings to withstand high voltage spikes in power supply and motor control applications

PHOENIX, Ariz. – Feb 1, 2010– ON Semiconductor (Nasdaq: ONNN) a premier supplier of high performance, energy efficient silicon solutions for green electronics has expanded its N-channel power MOSFET portfolio with the addition of 12 new 100 volt (V) devices. With industry-leading avalanche ratings of up to 500 millijoules (mJ), ON Semiconductor’s fully tested N-channel power MOSFETs are ideal for use in designs where voltage overstress resulting from unclamped inductive loads is a concern.

Download: JPG - 493.9kB  

Related Products:  NTP6411AN  NTD6416AN 


Low-side protected MOSFET photo
Automotive-Qualified Self Protected Low-Side Driver ICs

NCV840x family of devices in SOT-223, DPAK and SOIC8 packaging provides robust and reliable drive functionality in harsh automotive and industrial environments

PHOENIX, Ariz. – Dec. 11, 2009 – ON Semiconductor (Nasdaq: ONNN) introduced a family of low-side protected MOSFETs that feature high levels of integrated protection. Qualified in accordance with the AEC-Q101 standard, devices in the NCV840x family are ideal for use in switching applications operating in harsh automotive and industrial environments.

Download: JPG - 549.5kB  

Related Products:  NCV8402  NCV8403 


24 new 30 volt (V), N-channel Trench MOSFETs in DPAK, SO-8FL, µ8FL, and SOIC-8 packages featuring enhanced switching performance for synchronous buck converters.
New High-Density Trench MOSFETs for Computing and Game Console

New NTD49xx, NTMFS49x, NTTFS49x and NTMS49x series of 30 volt, N-channel devices improve switching performance and overall power efficiency

PHOENIX, Ariz. – Oct. 26, 2009 - ON Semiconductor (Nasdaq: ONNN), a leading global supplier of high performance, energy efficient, silicon solutions, has introduced 24 new 30 volt (V), N-channel Trench MOSFETs in DPAK, SO-8FL, µ8FL, and SOIC-8 packages featuring enhanced switching performance for synchronous buck converters in computing and game console applications.

Download: JPG - 577.8kB  

Related Product:  NTTFS4932N 


Dual-channel digital potentiometers with 256 resistor taps for fine resolution adjustment and an I2C-compatible interface for maximum interoperability.
New 256-Tap Digital Potentiometers for Control of Up to 16 Devices on One Bus

New devices offer volatile wiper register for applications using MCU with on-chip memory for wiper recall, or systems not requiring memory

PHOENIX, Ariz. – Oct. 13, 2009 – ON Semiconductor (Nasdaq: ONNN) a leading global supplier of high performance, energy efficient silicon solutions, today announced the availability of two new Digitally Programmable Potentiometer (DPP™) ICs suitable for high accuracy and stability for variable resistance adjustment applications in a wide range of industrial and consumer products. The CAT5270 and CAT5271 are dual-channel digital potentiometers with 256 resistor taps for fine resolution adjustment and an I2C-compatible interface for maximum interoperability. The new ON Semiconductor DPPs feature a volatile wiper register making them ideal for applications using a microcontroller (MCU) with on-chip memory for wiper recall, or for systems that do not require memory.

Download: JPG - 541.7kB  

Related Products:  CAT5271  CAT5270 


NCP2830 Class D Audio Amplifier
New Class D Audio Amplifier with an integrated charge pump

NCP2830 delivers constant 1 watt to deliver continuous high quality audio output as battery depletes

Phoenix, Ariz. - September 29, 2009 - ON Semiconductor (Nasdaq: ONNN), a leading global supplier of high performance, energy efficient, silicon solutions has introduced a new Class D Audio Amplifier with an integrated charge pump that provides a cost-effective and space-efficient speaker amplifier solution for applications such as cell phones, digital video recorders and portable speakers.

Download: JPG - 545.5kB  

Related Product:  NCP2830 


NP-MC series - A new family of ultra-low capacitance Thyristor Surge Protection Devices (TSPDs)
New Ultra-Low Capacitance Thyristor Surge Protection Devices

The NP-MC series offers performance, cost and space-saving benefits to designers of high-speed telecom equipment

PHOENIX, Ariz. - September 24, 2009 - ON Semiconductor (Nasdaq: ONNN), a leading global supplier of high performance, energy efficient, silicon solutions, has introduced the NP-MC series - a new family of ultra-low capacitance Thyristor Surge Protection Devices (TSPDs) that provide protection to sensitive electronic equipment from transient overvoltage conditions. With capacitance values 40 to 50 percent lower than existing products on the market, the NP-MC devices provide protection with minimal signal distortion in high-speed xDSL, T1/E1 and other broadband data transmission equipment.

Download: JPG - 661.7kB  

Related Product:  NP0080TA SERIES 


Power Line Carrier (PLC) Modem
Fully Integrated Power Line Modem for Smart Meters

New power line carrier modem integrates a modem and microcontroller to provide a robust low power, single chip solution

PHOENIX, Ariz. – Sept. 1, 2009 - ON Semiconductor (Nasdaq: ONNN), a leading global supplier of high performance, energy efficient, silicon solutions, has introduced the AMIS-49587, the latest member of the company’s power line carrier (PLC) modem family. The AMIS-49587 provides a highly integrated, standard compliant, low power PLC solution for use in applications such as smart electric automatic meter reading and management, street lighting control, smart power plug and building automation. Utilizing ON Semiconductor’s mixed-signal technology allows the AMIS-49587 to combine both the analog modem front end and digital post processing capability in the same integrated circuit.

Download: JPG - 895.4kB  

Related Product:  AMIS-49587 


Schottky barrier diodes
Industry's Smallest 30 V Schottky Barrier Diodes

New chip-level packaged Schottky diodes achieve 100 percent space utilization and offer best-in-class electrical performance

Phoenix, Ariz. - August 19, 2009 - ON Semiconductor (Nasdaq: ONNN), a leading global supplier of high performance, energy efficient, silicon solutions, has introduced four new 30 volt (V) Schottky barrier diodes. Housed in an ultra-small 0201 Dual Silicon No-lead (DSN2) chip level package, the new Schottky barrier diodes offer portable electronics designers both the industry’s smallest Schottky diode and best-in-class space-performance.

Download: JPG - 497.5kB  


High-Resolution I2C- and SPI-Compatible Digital Potentiometers
High-Resolution I2C- and SPI-Compatible Digital Potentiometers

256-tap Digitally Programmable Potentiometer (DPP™) ICs with 50 kΩ and 100 kΩ resistance options deliver enhanced stability and reliability

Phoenix, Ariz. – June 11, 2009 - ON Semiconductor (Nasdaq: ONNN), a leading global supplier of high performance, energy efficient, silicon solutions, has further expanded its family of Digitally Programmable Potentiometer (DPP™) ICs with new high-resolution devices incorporating I2C and Serial Peripheral Interface (SPI) Bus connectivity. The new DPPs offer a low-noise, reliable and space-saving alternative to mechanical potentiometers in applications ranging from instrumentation and industrial automation to portable battery-powered equipment.

Download: JPG - 491.0kB  


Integrated common mode choke and electrostatic discharge (ESD) protection IC
Industry’s First Common Mode Choke EMI Filter

New miniature device eliminates common mode noise in LVDS-class interfaces where high bandwidth prevents the use of traditional EMI filters

PHOENIX, Ariz.– May 27, 2009 – ON Semiconductor (Nasdaq: ONNN), a leading global supplier of high performance, energy efficient, silicon solutions, today introduced the industry’s first integrated common mode choke and electrostatic discharge (ESD) protection IC for high-speed data line applications.

Download: JPG - 828.7kB  

Related Product:  NUC2401 


CAT5140 digital potentiometer
256-Tap Digital Potentiometer with I²C Interface and Integrated EEPROM

CAT5140: Digitally Programmable Potentiometer (DPP™) with 50 kΩ and 100 kΩ end-to-end resistance

Phoenix, Ariz. – May 14, 2009 - ON Semiconductor (Nasdaq: ONNN), a leading global supplier of high performance, energy efficient, silicon solutions has added a new 256-tap, single-channel linear-taper device to its extensive family of Digitally Programmable Potentiometers (DPP™). The CAT5140 digital potentiometer is a low-noise, reliable and space-saving alternative to DACs and mechanical potentiometers. It features an on-chip, 8-bit, non-volatile EEPROM memory, which allows designers to calibrate once and retain the wiper setting in memory on power-up. The new DPP™ also provides five additional non-volatile registers for general purpose data storage, as well as a volatile wiper register for applications requiring temporary storage.

Download: JPG - 618.3kB  

Related Product:  CAT5140 


110 nm technology 'System Platform'
ASIC Offerings Expanded with 110 nm Technology and IP

Agreement with LSI Corporation utilizes 110 nm process, silicon-proven IP and flexible support options to minimize cost and time-to-market for advanced ASICs and SoCs

PHOENIX, Ariz. – April 13, 2009 - ON Semiconductor (Nasdaq: ONNN) a leading global supplier of high performance, energy efficient, silicon solutions today announced the further expansion of its application specific integrated circuit (ASIC) offering through an agreement with LSI Corporation (NYSE: LSI). The agreement gives ON Semiconductor customers access to an established and cost-effective 110 nanometer (nm) process technology and associated silicon-proven intellectual property (IP) via ON Semiconductor’s wafer fabrication facility in Gresham, Oregon.

Download: JPG - 580.4kB  


White LED Driver, High Efficiency, Charge Pump Converter Image
White LED Driver, High Efficiency, Charge Pump Converter

Related Product:  NCP5603 


Translator, AnyLevel™ Positive Input to NECL Output Voltage Image
Translator, AnyLevel™ Positive Input to NECL Output Voltage

Related Product:  NB100LVEP91 


Translator, 10-bit LVTTL / LVCMOS to LVPECL Image
Translator, 10-bit LVTTL / LVCMOS to LVPECL

Related Product:  MC100EPT622 


Transient Voltage Suppressor, Low Capacitance, for High Speed Data Interfaces Image
Transient Voltage Suppressor, Low Capacitance, for High Speed Data Interfaces

Related Product:  NUP4201 


Temperature Sensor with EEPROM Memory Image
Temperature Sensor with EEPROM Memory

Related Product:  CAT34TS02 


Stepper Motor Driver and Controller with I2C Bus, Microstepping Features and Stall Detection Image
Stepper Motor Driver and Controller with I2C Bus, Microstepping Features and Stall Detection

Related Product:  AMIS-30622 


Solution nav-green-load switches

icon for strata developer tools


Single Stage Power Factor Correction Controller Image
Single Stage Power Factor Correction Controller

Related Product:  NCP1651 


SiGe Differential Driver / Receiver with Variable Output Swing Image
SiGe Differential Driver / Receiver with Variable Output Swing

Related Product:  NBSG16VS 


SiGe Clock / Data Fanout Buffer, 1:4 Differential, 2.5 V / 3.3 V, with RSECL Outputs Image
SiGe Clock / Data Fanout Buffer, 1:4 Differential, 2.5 V / 3.3 V, with RSECL Outputs

Related Product:  NBSG14 


Preconfigured DSP System for Hearing Aids Image
Preconfigured DSP System for Hearing Aids

Related Product:  RHYTHM R3920 


Precision Operational Amplifier, 2 MHz Bandwidth, Low Noise, Zero-Drift, 25 µV Offset

Download: JPG - 64.0kB  

Related Product:  NCS21911 


Power Over Ethernet – Powered Device Interface Controller

Download: JPG - 21.4kB  

Related Products:  NCP1095  NCP1096 


Power MOSFET 40 V, 342 A, 0.75 mΩ, Single N−Channel SO-8FL Logic Level Image
Power MOSFET 40 V, 342 A, 0.75 mΩ, Single N−Channel SO-8FL Logic Level

Related Product:  NTMFS5C404NL 


Power MOSFET 40 V, 0.75 mΩ, 352 A, Single N−Channel Image
Power MOSFET 40 V, 0.75 mΩ, 352 A, Single N−Channel

Related Product:  NTMFS5C404NLT 


Power MOSFET 20V 3.9A 80 mOhm Complementary ChipFET Image
Power MOSFET 20V 3.9A 80 mOhm Complementary ChipFET

Related Product:  NTHC5513 


Power MOSFET -20V -7.7A 40 mOhm Single P-Channel WDFN6 Image
Power MOSFET -20V -7.7A 40 mOhm Single P-Channel WDFN6

Related Product:  NTLJS3113P 


Power MOSFET -20V -3.3A 100 mOhm Dual P-Channel WDFN6 Image
Power MOSFET -20V -3.3A 100 mOhm Dual P-Channel WDFN6

Related Product:  NTLJD3115P 


Power Line Carrier Modem Image
Power Line Carrier Modem

Related Product:  NCN49599 


Power Factor Correction Controller Image
Power Factor Correction Controller

Related Product:  NCP1650 


Power Factor Controller, Enhanced, High Efficiency Image
Power Factor Controller, Enhanced, High Efficiency

Related Product:  NCP1611 


Positive Overvoltage Protection Circuit with Internal Low Ron NMOS FET and Status Flag Image
Positive Overvoltage Protection Circuit with Internal Low Ron NMOS FET and Status Flag

Related Product:  NCP347 


PWM Controller, Fixed Frequency, Current Mode Image
PWM Controller, Fixed Frequency, Current Mode

Related Product:  NCP1216 


PLL Synthesized Clock Generator, Programmable, 3.3 V / 5.0 V (25 to 400 MHz) Image
PLL Synthesized Clock Generator, Programmable, 3.3 V / 5.0 V (25 to 400 MHz)

Related Product:  NBC12429 


PLL Clock Synthesizer, Multiprotocol, 3.3 V Serial Input, with Differential LVPECL Output Image
PLL Clock Synthesizer, Multiprotocol, 3.3 V Serial Input, with Differential LVPECL Output

Related Product:  NB4N441 


PLC Line Driver, 2 Amp Image
PLC Line Driver, 2 Amp

Related Product:  NCS5651 


Overvoltage Protection Circuit, USB Positive, with Internal PMOS FET and Overcurrent Protection Image
Overvoltage Protection Circuit, USB Positive, with Internal PMOS FET and Overcurrent Protection

Related Product:  NCP361 


Optical Image Stabilization (OIS) / Auto Focus (AF) Controller & Driver Image
Optical Image Stabilization (OIS) / Auto Focus (AF) Controller & Driver

Related Product:  LC898123AXD 


Power Factor Corrected Quasi-Resonant Primary Side Current Mode Controller for LED Lighting
ON Semiconductor Introduces Two New Series of Power Factor Corrected Ac-Dc Drivers for LED Lighting Applications

Extends single stage solutions with high power factor capability and broadens two stage solutions up to 150 watts

PHOENIX, Ariz. – Dec. 15, 2014 – ON Semiconductor (Nasdaq: ONNN), driving energy efficient innovations, announces two new series of power factor corrected (PFC) offline Ac-Dc drivers for high performance LED lighting applications. Extending the NCL3008x family of products, the NCL30085, NCL30086 and NCL30088 address single stage design implementations up to 60 watts (W) that require high power factor. The NCL30030 broadens the existing solutions which support higher power (up to 150 W) two stage topologies that require low optical ripple and wide LED forward voltage variation.

Download: JPG - 480.3kB  JPG - 69.4kB  

Related Product:  NCL30088 


Multilevel Input to CML Clock/Data Receiver/ Driver/Translator Buffer Image
Multilevel Input to CML Clock/Data Receiver/ Driver/Translator Buffer

Related Product:  NBSG16M 


Multi-Phase Controller with Dual Loop Capability, Configurable, DrMOS Compatible Image
Multi-Phase Controller with Dual Loop Capability, Configurable, DrMOS Compatible

Related Product:  NCP81232 


Multi Level Clock/Data Input to RSECL High Gain Receiver/Buffer/ Translator with Internal Termination Image
Multi Level Clock/Data Input to RSECL High Gain Receiver/Buffer/ Translator with Internal Termination

Related Product:  NB7L216 


Microstepping Motor Driver and Controller with LIN Bus and Stall Detection Image
Microstepping Motor Driver and Controller with LIN Bus and Stall Detection

Related Product:  AMIS-30623 


Microstepping Motor Driver and Controller image
Microstepping Motor Driver and Controller with LIN Bus

Related Product:  AMIS-30621 


Microstepping Motor Driver and Controller with I2C Bus and Stall Detection Image
Microstepping Motor Driver and Controller with I2C Bus and Stall Detection

Related Product:  AMIS-30624 


MOSFET / IGBT Drivers, High Voltage, High and Low Side, Dual Input Image
MOSFET / IGBT Drivers, High Voltage, High and Low Side, Dual Input

Related Product:  NCP5181 


Low Power & High-Resolution Audio Processing System LSI

Low Power & High-Resolution Audio Processing System LSI

Related Product:  LC823455 


Low Power & High-Resolution Audio Processing System LSI Image
Low Power & High-Resolution Audio Processing System LSI

Related Product:  LC823450 


Linear Voltage Regulator, LDO, Very Low Iq Image
Linear Voltage Regulator, LDO, Very Low Iq

Related Product:  NCV8664 


Linear Voltage Regulator, LDO, Tri-Mode, Low Iq, 200 mA Image
Linear Voltage Regulator, LDO, Tri-Mode, Low Iq, 200 mA

Related Product:  NCP584 


Linear Voltage Regulator, LDO, Dual Output, 250 mA Image
Linear Voltage Regulator, LDO, Dual Output, 250 mA

Related Product:  NCP5504 


Linear Voltage Regulator, LDO, 250 mA Image
Linear Voltage Regulator, LDO, 250 mA

Related Product:  NCV5504 


Linear Voltage Regulator, LDO, 150 mA Image
Linear Voltage Regulator, LDO, 150 mA

Related Product:  NCV4299 


Linear Regulator, Very-Wide Input Voltage Range, 450 V, 10 mA Image
Linear Regulator, Very-Wide Input Voltage Range, 450 V, 10 mA

Related Product:  NCP785A 


LED Driver, High Efficiency, Single Stage, Power Factor Corrected Image
LED Driver, High Efficiency, Single Stage, Power Factor Corrected

Related Product:  NCL30001 


LED Driver, Charge Pump, 2-Channel Imgae
LED Driver, Charge Pump, 2-Channel

Related Product:  CAT3224 


LED Driver Controller, Fixed, Off Time, Switch Mode Image
LED Driver Controller, Fixed, Off Time, Switch Mode

Related Product:  NCL30100 


LED Controller, 6-Channel, with Fault Diagnostics Image
LED Controller, 6-Channel, with Fault Diagnostics

Related Product:  CAT4026 


KNX Transceiver for Twisted Pair Networks Image
KNX Transceiver for Twisted Pair Networks

Related Products:  NCN5110  NCN5121  NCN5130 


KNX Transceiver for Twisted Pair Networks Image
KNX Transceiver for Twisted Pair Networks

Related Product:  NCN5120 


Interline Transfer EMCCD Image Sensor, 4.4 MP Image
Interline Transfer EMCCD Image Sensor, 4.4 MP

Related Product:  KAE-04471 


Interline Transfer EMCCD Image Sensor, 2.1 MP Image
Interline Transfer EMCCD Image Sensor, 2.1 MP

Related Product:  KAE-02152 


Interline Transfer EMCCD Image Sensor, 2.1 MP Image
Interline Transfer EMCCD Image Sensor, 2.1 MP

Related Product:  KAE-02150 


Interline Transfer CCD Image Sensor, 8.6 MP Image
Interline Transfer CCD Image Sensor, 8.6 MP

Related Product:  KAI-08670 


Integrated PoE-PD and DC-DC Converter Controller, 40 W, with Auxiliary Supply Support Image
Integrated PoE-PD and DC-DC Converter Controller, 40 W, with Auxiliary Supply Support

Related Product:  NCP1083 


Integrated PoE-PD and DC-DC Converter Controller, 13 W, with Auxiliary Supply Support Image
Integrated PoE-PD and DC-DC Converter Controller, 13 W, with Auxiliary Supply Support

Related Product:  NCP1082 


Integrated DC-DC Converter for PoE and Telecom Image
Integrated DC-DC Converter for PoE and Telecom

Related Product:  NCP1030 


High Speed 5A Dual Low Side MOSFET driver Image
High Speed 5A Dual Low Side MOSFET driver

Related Product:  NCP81071 


High Performance, 650 V Half Bridge Gate Driver for GaN Power Switches

Download: JPG - 45.1kB  

Related Product:  NCP51820 


High Current Synchronous Buck Converter Image
High Current Synchronous Buck Converter

Related Product:  NCP3231 


Hex Low-side MOSFET Predriver Image
Hex Low-side MOSFET Predriver

Related Product:  NCV7513 


Hex Half-Bridge Driver Image
Hex Half-Bridge Driver

Related Product:  NCV7718 


Electronic Fuse Image
Electronic Fuse

Related Product:  NIS5112 


ESD Protection Diode, Ultra Low Capacitance, Unidirectional Image
ESD Protection Diode, Ultra Low Capacitance, Unidirectional

Download: JPG - 72.9kB  

Related Product:  ESD9L 


ESD Protection Diode, Bi-directional, SOD-323 Image
ESD Protection Diode, Bi-directional, SOD-323

Related Product:  SD12C 


ESD Protection Array, Ultra Low Capacitance, for High Speed Data Lines Image
ESD Protection Array, Ultra Low Capacitance, for High Speed Data Lines

Related Product:  NUP4016 


Dual SPST Analog Switch, Single Supply Image
Dual SPST Analog Switch, Single Supply

Download: JPG - 45.0kB  

Related Product:  NLAS323 


Current-Shunt Monitors, Voltage Output, Bidirectional, Zero-Drift, Low or High-Side Current Sensing Image
Current-Shunt Monitors, Voltage Output, Bidirectional, Zero-Drift, Low or High-Side Current Sensing

Related Products:  NCS210R  NCS211R  NCS213R  NCS214R  NCS199A1R  NCS199A2R  NCS199A3R 


Current Mode Resonant Controller with Integrated High Voltage Drivers, High Performance Image
Current Mode Resonant Controller with Integrated High Voltage Drivers, High Performance

Related Product:  NCP1399 


Crystal Oscillator Module, PureEdge™, 156.25 MHz / 312.50 MHz LVPECL, 3.3 V Image
Crystal Oscillator Module, PureEdge™, 156.25 MHz / 312.50 MHz LVPECL, 3.3 V

Related Product:  NBXDBA017 


Controller, Variable Off-Time Current Mode, with Short Circuit Protection Image
Controller, Variable Off-Time Current Mode, with Short Circuit Protection

Related Product:  NCP1351 


Controller, PoE-PD Interface, Integrated Image
Controller, PoE-PD Interface, Integrated

Related Product:  NCP1090 


Controller, High Performance Resonant Mode, with High and Low Side Drivers Image
Controller, High Performance Resonant Mode, with High and Low Side Drivers

Related Product:  NCP1396 


Controller, High Performance Resonant Mode Image
Controller, High Performance Resonant Mode

Related Product:  NCP1395 


Comtrend GRG-4281 GPON Gateway
Comtrend introduced a new Wi-Fi 6 product line

Download: PNG - 34.2kB  


Clock Multiplier, LVPECL / LVCMOS, Programmable, 3.3 V Image
Clock Multiplier, LVPECL / LVCMOS, Programmable, 3.3 V

Related Product:  NB3N3020 


Clock Fanout Buffer, 1:21 Differential, 3.3 V, with HCSL Level Output Image
Clock Fanout Buffer, 1:21 Differential, 3.3 V, with HCSL Level Output

Related Product:  NB4N121K 


Clock Driver, 2:1:9 Differential HSTL / PECL to HSTL, 3.3 V Image
Clock Driver, 2:1:9 Differential HSTL / PECL to HSTL, 3.3 V

Related Product:  MC100EP809 


Clock / Data Fanout Buffer, 2:1:20 Differential, HSTL / ECL / PECL, 2.5 V / 3.3 V Image
Clock / Data Fanout Buffer, 2:1:20 Differential, HSTL / ECL / PECL, 2.5 V / 3.3 V

Related Product:  NB100LVEP221 


Clock / Data Fanout Buffer, 1:4 AnyLevel™ Input, LVDS, 3.3 V Image
Clock / Data Fanout Buffer, 1:4 AnyLevel™ Input, LVDS, 3.3 V

Related Product:  NB6N14S 


CMOS Image Sensor, Global Shutter, 1.3 MP (SXGA) Image
CMOS Image Sensor, Global Shutter, 1.3 MP (SXGA)

Related Product:  PYTHON1300 


CAN Transceiver, High Speed, Low Power Image
CAN Transceiver, High Speed, Low Power

Download: JPG - 67.2kB  

Related Product:  NCV7341 


CAN Transceiver, High Speed, Low Power Image
CAN Transceiver, High Speed, Low Power

Related Product:  NCV7340 


Buck Converter, DC-DC, Dual, Low Iq, High Efficiency, 2.25 MHz, 1.6 A Image
Buck Converter, DC-DC, Dual, Low Iq, High Efficiency, 2.25 MHz, 1.6 A

Related Product:  NCP1532 


Buck / Boost / Inverting Regulator, Switching, Constant Current, 1.5 A, for HB-LEDs with Enable Image
Buck / Boost / Inverting Regulator, Switching, Constant Current, 1.5 A, for HB-LEDs with Enable

Related Product:  NCP3066 


Boost Converter, PFM, DC-DC, 25 V, 25 mA Image
Boost Converter, PFM, DC-DC, 25 V, 25 mA

Related Product:  NCP1406 


Boost Converter, PFM, DC-DC, 15 V, 50 mA Image
Boost Converter, PFM, DC-DC, 15 V, 50 mA

Related Product:  NCP1403 


Audio Power Amplifier, Stereo Headphone 135 mW Image
Audio Power Amplifier, Stereo Headphone 135 mW

Related Product:  NCP2809 


Audio Power Amplifier, Class D, 2.65 W, Filterless, Mono Image
Audio Power Amplifier, Class D, 2.65 W, Filterless, Mono

Related Product:  NCP2820 


Audio Power Amplifier, 1.8 Watt, with Selectable Shutdown Image
Audio Power Amplifier, 1.8 Watt, with Selectable Shutdown

Related Product:  NCP4894 


Audio Power Amplifier, 1.0 W Image
Audio Power Amplifier, 1.0 W

Related Product:  NCP2890 


Analog Switch, Ultra Small, Dual Single Pole, Single Throw, with Over Voltage Tolerance Image
Analog Switch, Ultra Small, Dual Single Pole, Single Throw, with Over Voltage Tolerance

Related Product:  NLAS2066 


AXM0F243 Narrow-Band RF Transceiver System-on-Chip (SoC)

Download: JPG - 507.2kB  

Related Product:  AXM0F243 


512-Kb SPI Serial CMOS EEPROM Image
512-Kb SPI Serial CMOS EEPROM

Related Product:  CAT25512 


450 mA LDO Linear Voltage Regulator with Reset and Delay Image
450 mA LDO Linear Voltage Regulator with Reset and Delay

Related Product:  NCV4275 


3.3 V ECL Programmable Delay Chip Image
3.3 V ECL Programmable Delay Chip

Related Product:  MC100EP196 


2.9V to 5.5V, 5A Integrated Synchronous DC-DC Step Down Converter Image
2.9V to 5.5V, 5A Integrated Synchronous DC-DC Step Down Converter

Related Product:  NCP3135 


2.5 to 5.5 V ECL D Flip-flop w/Differential Reset & Input Termination Image
2.5 to 5.5 V ECL D Flip-flop w/Differential Reset & Input Termination

Related Product:  NB4L52 


2.3 MP 1/2.7 CMOS Image Sensor
2.3 MP 1/2.7 CMOS Image Sensor

Related Product:  AR0231AT 


2 x 2 Crosspoint Switch, SiGe Differential, 2.5 V / 3.3 V, with Ouput Level Select Image
2 x 2 Crosspoint Switch, SiGe Differential, 2.5 V / 3.3 V, with Ouput Level Select

Related Product:  NBSG72A 


2 MHz Non-Synchronous SEPIC / Boost Controller Image
2 MHz Non-Synchronous SEPIC / Boost Controller

Related Product:  NCV898031 


150 mA CMOS Low Iq LDO Voltage Regulator with Voltage Detector Output Image
150 mA CMOS Low Iq LDO Voltage Regulator with Voltage Detector Output

Related Product:  NCP400 


13 MP 1/3
13 MP 1/3" CMOS Image Sensor

Related Product:  AR1335 


100 V Synchronous Buck Controller Image
100 V Synchronous Buck Controller

Related Product:  NCP1034 


1 Mb SPI Serial CMOS EEPROM Image
1 Mb SPI Serial CMOS EEPROM

Related Product:  CAT25M01 


Download: JPG - 437.5kB  JPG - 401.3kB  


Download: JPG - 70.6kB  


Related Product:  NCP1090 




Related Product:  NCP1092 


Download: JPG - 65.8kB  

Related Product:  NCP1094 


Related Product:  NCP1091 


Download: JPG - 65.8kB  

Related Product:  NCP1093 


Download: JPG - 591.3kB  

Related Product:  EZAIRO 8300 


Download: JPG - 353.3kB  



Your request has been submitted for approval.
Please allow 2-5 business days for a response.
You will receive an email when your request is approved.
Request for this document already exists and is waiting for approval.